Other Parts Discussed in Thread: TEST2
Hi,
Actually I am working with the DM816x EVM to figure out how to do the initial board bring-up for our custom board. I have configured MBOOT[4:0] pins to 00111 so Ethernet(GMII) is the first boot mode. I removed the SD card. An Ethernet cable is connected between the EVM and my PC. The PC runs VirtualBox with Ubuntu 10.04. When powering the board, it does not boot, however I can see DHCP requests and DHCP ACK transactions using Wireshark.
In the last two weeks I have read a lot of wiki pages and posts, tried so many things but still could not find the root cause of my problem. Can somobody tells me which setup is required to boot U-boot from Ethernet or at least where to find more info?
Kind regards,
Julie