This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713 MCASP



Hello,

         Now i am working with a TMS320C6713,  i want to receive data and send data through the MCASP port,  i had write the program, when i run the program i can't send data by TDM mode,but i can send data by burst mode and i can receive data no matter MCASP working with TDM mode or burst mode. i check my program and my MCASP setup and Initialization is follow the SPRU041J-November 2008, i can see all the clock(ACLK X,AHCLKX,AFSX) signal by the oscilloscope,when work at the burst mode i can detect the data output which i hope send.but i set the XMOD bit(2~20h) hope it work on TDM mode,i can not detect the data output which i hope send,i can see the data by  the memory (the address of the XBUF),examine the XSTAT find the XDATA bit is zero(XBUF is written and is full.),who can  tell me why? thinks