This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Artifacts in SW Mosaic dual window on 816x SDK 5.04



Hi,

I have following omx pipeline : File(H264 1080p30) ->Decoder->DEI->SWMosaic(1080p30)->Display

                                                                                                        |->Encoder

I am using 2 files (e.g 2  pipelines using same DEI and SWMosaic components , but different channels) play and place them in SWMosaic as 2 windows. Initially I have 2 overlapping windows 1080p each , which looks just fine.

Then I use re-size in DEI and I use CreateLayout setconfig to changel ayout parameters for mosaic for different window size and placement. These changes are done dynamically while all the components in Executing state. The re-size and window movement are fine.

The problem is that second window become blueish after couple of size and place change. Another thing is that I see the leftovers of first window movie on the top of the second movie playing it looks almost like a projection of part of the first movie. These happenes only if I change size and placement dynamicaly.

The same issue observed also with 5.03 SDK. I am attaching screenshot picture of these problem :

.