Other Parts Discussed in Thread: TMS320C6678
I want to interface my FPGA with the TMS320C6678 and want some input on the best way to interface the two devices. I've been using the TigerSharc from ADI which has an external 64-bit data bus, 32-bit address bus, chip select and read/write signals. Pretty simple interface and easy to code in the FPGA. I don't see such an interface with the TI processors. If anyone has done a design that interfaces such devices can you please share what you did?
Respectfully,
joe