Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which DSP Dev Kit and ADC module should I buy?

Other Parts Discussed in Thread: ADS4125EVM, ADS7863EVM

Hello,

I am looking for advice on which DSP development kit should I buy? I hope to interface the DSP kit to a single channel 12 bit, 100 MSPS ADC module. I do not plan to build any hardware or use an FPGA to do this. I am planning to perform FFT on the signal.

Regards,

Anthony

  • A quick search of the product information shows that TI manufactures 17 active A/D converter ICs with 12 bits of resolution and sampling rate limits of 105 to 250 MSPS, typically with LVDS output.  They have evaluation modules, e.g. ADS4125EVM, but these modules are usually compatible with the deserializer TSW1200EVM (which is meant to interface with a TSW1100 analysis tool or with a PC) and *not* ready for direct attachment to DSP Starter Kits.

    I suspect that even with the fastest TI DSPs, you'll have trouble sustaining Fourier transformation at a rate of 100 MSPS, especially if you need to send the result somewhere, and at any rate you'd need to adapt the A/D EVM to work with the DSP in parallel output mode, since there is no way the TMS320Cxxxx DSKs can process serial data at a 1200 Mbit/s rate.  (I don't think you can even route signals of that frequency reliably thbrough the inter-board connectors.)  There are several slower A/D EVMs designed for use with DSP Starter Kits via the 5/6K Interface board, e.g. ADS7863EVM (500KSPS).  There is also a THS1206EVM (6MSPS aggregate, 2 or 4 channels) with parallel output instead of serial output.  You might consider whether you really need to operate at such a high sampling rate, and if you do, perhaps instead of a DSK you should use the ADC_EVM->TSW1200EVM->PC setup to store and analyze the raw data on the PC.

  • Douglas, Thanks. Your advice is much appreciated. Anthony