Hi,
Could TI recommend a type of external circuit/device to drive DEEPSLEEP low in the process of turning OMAP L138 into deep sleep mode?
In “10.10.1 Entering Deep Sleep Mode” of L138 TRM, although for waking the chip up from deep sleep one can both use an external signal or RTC, for putting the device INTO deep sleep however one must uses an external signal to drive DEEPSLEEP low to complete the final step.
Which circuit/device should be used to do this final step?
One option I know is to use a cheap MSP430, and its internal timer could guarantee sufficient delay so that it could work in conjunction with L138 to put L138 into deepsleep.
Another option might be use some circuit combination, for example a MOSFET with some other component, to somehow create a delay before it starts putting DEEPSLEEP pin low.
Since MSP430 chips are very cheap and its performance is guaranteed, it seems more attractive than using circuit solution since the later requires accurate calculation, among other considerations.
We would like to know which method, or a better one, does TI recommend?
Paul