This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About C6678 DDR3 DDRSLRATE[1:0]

Guru 15520 points

Hi,

I have a question about C6678 DDR3 DDRSLRATE[1:0] pin.

I'm looking at Hardware Design Guide page.95 Table24 Slew Rate Control.
There are 4 combination for DDRSLRATE[1:0] but I can't decide which
combination is the best for customer board.

From Hardware Design Guide and DDR3 Design Guide,
I can't decide which combination of DDRSLRATE[1:0] to select.

Is there any information which I could refer to
for deciding the combination?

best regards,
g.f.