This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Additional sources ISO image documentation

Expert 1060 points


 

Hi, experts.

There are ezsdk_5_05_01_04_sources.iso in dm8148 download page.

http://software-dl.ti.com/dsps/dsps_public_sw/ezsdk/latest/index_FDS.html

When I open the iso image file, there are many patch and folder. But it is not intuitive to use.

I would like to know it's usage. Is there any documentation describing this folder ?

Please explain how to use it.

 

Best regards.

Jay.

 

  • Hello,

    6. Additional Sources

    The EZSDK installer already comes with the sources of the TI software. If you want to download the additional source files of the open source components, download them below as an ISO image (Additional Sources). Note that this is an optional download which is not required to develop applications with the EZSDK.

    Best Regards,

    Margarita

  •  

    Hi, Margarita

     

    Thank you for the answer.

    I've already downloaded the additional source file.

    Is all the patch and folder just open source? no related with ezsdk from TI?

    Is there any document that explain those folder? I just want to know it's usage because it's hard to understand without docs.

     

    Best Regards.

    Jay.