Note: if this is the wrong forum please move.
Hello:
I am using CCS V5.3.0.00090, bios_5_42_00_07, xdctools_3_24_05_48
trying to build AER project aertest_c55l_C55L_COFF
All of the .c source files compile and when it tries to link I get the following...
'Building target: aertest_c55l_C55L_COFF.out'
'Invoking: C5500 Linker'
"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/bin/cl55" -v5509A -g --define=ti_targets_C55_large --define=xdc_target_types__=ti/targets/std.h --define=C5510 --define=c5509a --diag_suppress=1112 --diag_suppress=825 --diag_suppress=838 --diag_suppress=828 --diag_suppress=827 --diag_suppress=77 --diag_suppress=837 --diag_suppress=824 --diag_warning=225 --optimize_with_debug --ptrdiff_size=32 --algebraic --memory_model=large --std_lib_func_defined -k --c_src_interlist --output_all_syms -z -m"aertest_c55l_C55L_COFF.map" --stack_size=0x200 --heap_size=0x400 --warn_sections -i"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/lib" -i"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/lib" -i"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/include" --reread_libs --rom_model --sys_stacksize=0x200 -o "aertest_c55l_C55L_COFF.out" -l"./configPkg/linker.cmd" "./veuinstbuff.obj" "./siutx.obj" "./siurx.obj" "./siumss.obj" "./siudrc.obj" "./siuagc.obj" "./siuaer.obj" "./siu_multi_mic.obj" "./siu.obj" "./sgnsim.obj" "./piu.obj" "./drcinstbuff.obj" "./drcfilter.obj" "./agcinstbuff.obj" "./aerxbuff.obj" "./aerworkb.obj" "./aertxeqfb.obj" "./aersim_setup.obj" "./aersim_fileIO.obj" "./aersim.obj" "./aerrxtxscratch.obj" "./aerrxeqfb.obj" "./aerrxbsout.obj" "./aerrbuff.obj" "./aerpsiu.obj" "./aerpowbuff.obj" "./aerpbuff.obj" "./aernrbuff.obj" "./aernbuff.obj" "./aeriobuff.obj" "./aerinstbuff.obj" "./aerhupab.obj" "./aerhovfb.obj" "./aerhbuff.obj" "./aerfdnlps.obj" "./aerfdnlpb.obj" "./aerbsdlb2.obj" "./aerbsdlb.obj" "./aepsim.obj" -l"libc.a" "C:/ti/packages/ti/mas/aer/test/lnkr/c55l/aertest_c55l_ccs.cmd"
<Linking>
error: cannot find file "./configPkg/linker.cmd"
"C:/ti/packages/ti/mas/aer/test/lnkr/c55l/aertest_c55l_ccs.cmd", line 337: warning:
>> Compilation failure
no matching section
error: errors encountered during linking; "aertest_c55l_C55L_COFF.out" not
built
gmake: *** [aertest_c55l_C55L_COFF.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
I did a full directory file search of everything TI and only find...
C:\ti\packages\ti\mas\aer\test\aertest_c55l_C55L_COFF\Debug\configPkg\linker.cmd.cp
C:\ti\xdctools_3_24_05_48\packages\xdc\tools\configuro\template\linker.cmd.asm.xdt
C:\ti\bios_5_42_00_07\xdctools\packages\xdc\tools\configuro\template\linker.cmd.asm.xdt
Can anyone tell me where is or where to find ./configPkg/linker.cmd ?
Thanks