Hello,
We would like to use 512MB NAND flash with the DM3730 (CUS100 package). According to the datasheet it is possible to address up to 1GB. I even see multiple board with 1 512MB NAND: http://www.technexion.com/images/datasheets/tdm-3730.pdf
The device i want to use is the Micron MT29F4G08ABBEAH4.
However,when I open the reference manual i see this:
It says i can only do 256MB with one chip. Is there a way to avoid this issue? Or cvan the GPMC handle 512?