Other Parts Discussed in Thread: TPS65910
Hello everyone,
I've managed to boot a "small" rootfs from my nand ( ~32 MB ), by using UBIFS ( UBI-FruStrations? ). Now when I create a larger rootfs ( ~64 MB ) it boots the first time, but afterwards no more.
I've tried almost everything but nothing seems to help me! I notice read errors the first time, but it continues to boot... I really don't know what I'm doing wrong here and I'm getting really frustrated too because of this weird behaviour!
-- Ubinize.cfg
[RFS-volume]
mode=ubi
image=ubifs.img
vol_id=0
vol_size=192MiB
vol_type=dynamic
vol_name=rootfs
vol_flags=autoresize
commands i've used to create UBI:
mkfs.ubifs -r rootfs/ -o ubifs.img -m 2048 -e 126976 -c 1580 –F
ubinize -o ubi.img -m 2048 -p 128KiB -O 2048 ubinize.cfg
I write my ubi image from within uboot:
U-Boot# mw.b ${loadaddr} 0xFF {partition-size}
U-Boot# tftp ${loadaddr} ubi.img
U-boot# nand erase 0x00780000 {partition-size}
U-boot# nand write ${loadaddr} 0x00780000 {filesize}
...and afterwards boot from nand...
Booting from nand ...
NAND read: device 0 offset 0x280000, size 0x500000
5242880 bytes read: OK
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2843304 Bytes = 2.7 MiB
Load Address: 80008000
Entry Point: 80008000
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.077850] tps65910 1-002d: could not be detected
[ 0.404754] mtdoops: mtd device (mtddev=name/number) must be supplied
INIT: version 2.88 booting
Using makefile-style concurrent boot in runlevel S.
Setting the system clock.
Cannot access the Hardware Clock via any known method.
Use the --debug option to see the details of our search for an access method.
Unable to set System Clock to: Thu Jan 1 00:00:07 UTC 1970 ... (warning).
Activating swap...done.
Checking root file system...fsck from util-linux-ng 2.17.2
fsck: fsck.auto: not found
fsck: Error 2 while executing fsck.auto for /lib/init/rw/rootdev
done.
[ 8.200195] UBI error: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 495:51200, read 64 bytes
Setting the system clock.
Cannot access the Hardware Clock via any known method.
Use the --debug option to see the details of our search for an access method.
Unable to set System Clock to: Thu Jan 1 00:00:08 UTC 1970 ... (warning).
Cleaning up ifupdown....
Setting up networking....
[ 8.813323] UBI error: ubi_io_read: error -74 (ECC error) while reading 66 bytes from PEB 495:57120, read 66 bytes
[ 8.905944] UBI error: ubi_io_read: error -74 (ECC error) while reading 66 bytes from PEB 495:58672, read 66 bytes
[ 8.936309] UBI error: ubi_io_read: error -74 (ECC error) while reading 62 bytes from PEB 495:59064, read 62 bytes
[ 9.022216] UBI error: ubi_io_read: error -74 (ECC error) while reading 62 bytes from PEB 495:60616, read 62 bytes
[ 9.072296] UBI error: ubi_io_read: error -74 (ECC error) while reading 62 bytes from PEB 495:62384, read 62 bytes
Activating lvm and md swap...done.
Checking file systems...fsck from util-linux-ng 2.17.2
done.
Mounting local filesystems...done.
Activating swapfile swap...done.
Cleaning up temporary files...[ 9.483398] UBI error: ubi_io_read: error -74 (ECC error) while reading 63 bytes from PEB 495:65312, read 63 bytes
.
Cleaning up temporary files....
[ 9.938079] UBI error: ubi_io_read: error -74 (ECC error) while reading 63 bytes from PEB 495:66080, read 63 bytes
[ 9.953125] UBI error: ubi_io_read: error -74 (ECC error) while reading 63 bytes from PEB 495:66464, read 63 bytes
INIT: Entering runlevel: 2
Using makefile-style concurrent boot in runlevel 2.
[ 10.550659] UBI error: ubi_io_read: error -74 (ECC error) while reading 66 bytes from PEB 495:68992, read 66 bytes
Starting nginx: [ 10.899200] UBI error: ubi_io_read: error -74 (ECC error) while reading 74 bytes from PEB 495:71008, read 74 bytes
the configuration file /etc/nginx/nginx.conf syntax is ok
[emerg]: socket() [::]:80 failed (97: Address family not supported by protocol)
configuration file /etc/nginx/nginx.conf test failed
startpar: service(s) returned failure: nginx ... failed!
Debian GNU/Linux 6.0 wcap ttyO0
wcap login: root
Password:
Linux wcap 3.2.0 #8 Fri Jul 5 13:09:48 CEST 2013 armv7l
The programs included with the Debian GNU/Linux system are free software;
the exact distribution terms for each program are described in the
individual files in /usr/share/doc/*/copyright.
Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
permitted by applicable law.
root@wcap:~# reboot
Broadcast message from root@wcap (ttyO0) (Thu Jan 1 00:00:36 1970):
The system is going down for reboot NOW!
INIT: Sending proUsing makefile-style concurrent boot in runlevel 6.
Saving the system clock.
Cannot access the Hardware Clock via any known method.
Use the --debug option to see the details of our search for an access method.
Stopping nginx: nginx.
Asking all remaining processes to terminate...done.
All processes ended within 1 seconds....done.
Cleaning up ifupdown...[ 37.352661] UBI error: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 495:55184, read 64 bytes
.
Deactivating swap...done.
Will now restart.
[ 39.636932] Restarting system.
CCCCCCCC
U-Boot SPL 2013.01.01 (Jul 03 2013 - 15:25:44)
No AC power, disabling frequency switch
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
SF: Detected M25P32 with page size 64 KiB, total 4 MiB
U-Boot 2013.01.01 (Jul 05 2013 - 15:11:37)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
NAND: 512 MiB
Using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
Recovering from network ...
cpsw Waiting for PHY auto negotiation to complete......... TIMEOUT !
Using cpsw device
cpsw Waiting for PHY auto negotiation to complete......... TIMEOUT !
cpsw Waiting for PHY auto negotiation to complete......... TIMEOUT !
ARP Retry count exceeded; halting
ping failed; host 223.254.254.1 is not alive
Booting from nand ...
NAND read: device 0 offset 0x280000, size 0x500000
5242880 bytes read: OK
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2843304 Bytes = 2.7 MiB
Load Address: 80008000
Entry Point: 80008000
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.077911] tps65910 1-002d: could not be detected
[ 0.404907] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 5.595153] UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 3:4096, read 126976 bytes
[ 5.745269] UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 4:4096, read 126976 bytes
[ 5.760162] UBI error: ubi_io_read: error -74 (ECC error) while reading 11 bytes from PEB 10:14336, read 11 bytes
[ 5.771118] UBIFS error (pid 1): ubifs_leb_read: reading 11 bytes from LEB 8:10240 failed, error -74
[ 5.781890] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[ 5.790679] Backtrace:
[ 5.793365] [<c0018c00>] (dump_backtrace+0x0/0x10c) from [<c03a65f0>] (dump_stack+0x18/0x1c)
[ 5.802337] r7:00008000 r6:c05259fc r5:c0597388 r4:c0597388
[ 5.808410] [<c03a65d8>] (dump_stack+0x0/0x1c) from [<c03a6658>] (panic+0x64/0x198)
[ 5.816558] [<c03a65f4>] (panic+0x0/0x198) from [<c04f9d50>] (mount_block_root+0x1f8/0x2bc)
[ 5.825439] r3:00000000 r2:00000000 r1:cf01df78 r0:c046a568
[ 5.831512] [<c04f9b58>] (mount_block_root+0x0/0x2bc) from [<c04f9f10>] (prepare_namespace+0x94/0x1cc)
[ 5.841430] [<c04f9e7c>] (prepare_namespace+0x0/0x1cc) from [<c04f92f8>] (kernel_init+0xf0/0x124)
[ 5.850860] r5:c052e5cc r4:c05946c0
[ 5.854705] [<c04f9208>] (kernel_init+0x0/0x124) from [<c0043b6c>] (do_exit+0x0/0x69c)
[ 5.863128] r5:c04f9208 r4:00000000
Kind regards!