This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Im working on DM365 based ipnc camera with appro framework using ipnc 3.0 version. I know TI has provided the support to the processor for onvif and psia compliance. But i want to test the same on my camera. Please guide me through the available options and the procedures so that i can test them well in time.
Any help in this regard would be deeply appreciated . Thanx in advance
As I understand it, you need to use the Onvif Test Tool or PSIA conformance tool to run through their documented test procedure.
However, the IPNC does not support all of the actions and the process seems to be that you just ignore things it can't do.
Also, IPNC 3.0 is quiote old now, version 5.1 is available from Appro's FTP server although I've seen a few posts about problems so it may be better to try 4.0 or 4.1. There were updates to the ONVIF code in 5.0 so downloading both & running "diff" may be educational.
Thanx Bob,
It was indeed a great help.
and also to tell you im also working on ipnc 4 for a different project.
Hello Rohit ,
PLease use v5.1 as this is the latest version and has the latest fixes/updates.
Please do a compare and pick the fixes and updates that you need from v5.1
Regards,
Raghu
Hi Raghu,
Im using v5.1 SDk. For onvif conformity I would like to know that it supports v1.02 Onvif. How can I check which onvif profile does it support. I am looking forward to provide profile S to the cam. Also how can this conformity be proven to profile S.
Regards,
Rohit