Dear experts,
I am getting the following errors while booting the uImage which is build using the latest OMAP35x Linux PSP 02.01.01.08 2.6.29-rc3 kernel source.
I had flashed the u-boot, x-loader and ramdisk images which has taken from this release version.
I had given the following boot args in u-boot prompt as:
setenv bootargs mem=128M console=ttyS0,115200n8 noinitrd ip=<board_IP_address> rw root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock,rsize=4096,wsize=4096,proto=tc
The filesys is taken from this same PSP package.
Can anybody suggests me to solve this error
<6>Freeing init memory: 156K
Freeing init memory: 156K
INIT: version 2.86 booting
Starting udev<3>uncorrectable error : uncorrectable error : <3>uncorrectable error : <3>uncorrectable error : <3>end_request: I/O error, dev mtdblock0, sector 0
<3>end_request: I/O error, dev mtdblock0, sector 0
<3>Buffer I/O error on device mtdblock0, logical block 0
Buffer I/O error on device mtdblock0, logical block 0
<3>uncorrectable error : uncorrectable error : <3>end_request: I/O error, dev mtdblock0, sector 8
<3>end_request: I/O error, dev mtdblock0, sector 8
<3>Buffer I/O error on device mtdblock0, logical block 1
Buffer I/O error on device mtdblock0, logical block 1
<3>uncorrectable error : uncorrectable error : <3>end_request: I/O error, dev mtdblock0, sector 16
<3>end_request: I/O error, dev mtdblock0, sector 16
<3>Buffer I/O error on device mtdblock0, logical block 2
Buffer I/O error on device mtdblock0, logical block 2
<3>uncorrectable error : uncorrectable error : <3>end_request: I/O error, dev mtdblock0, sector 24
<3>end_request: I/O error, dev mtdblock0, sector 24
<3>Buffer I/O error on device mtdblock0, logical block 3
Buffer I/O error on device mtdblock0, logical block 3
<3>uncorrectable error : uncorrectable error : <3>uncorrectable error : <3>uncorrectable error : <3>end_request: I/O error, dev mtdblock0, sector 0
<3>end_request: I/O error, dev mtdblock0, sector 0
<3>Buffer I/O error on device mtdblock0, logical block 0
Buffer I/O error on device mtdblock0, logical block 0
and populating dev cachetar: can't open '/etc/dev.tar': Permission denied
mv: cannot rename '/tmp/uname': Permission denied
Remounting root file system...
root: mount: mounting rootfs on / failed: No such file or directory
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
/etc/init.d/rc: /etc/rcS.d/S37populate-volatile.sh: line 1: can't create /etc/volatile.cache: Permission denied
Setting up IP spoofing protection: rp_filter.
Configuring network interfaces... udhcpc (v1.13.2) started
Sending discover...