Dear Experts,
I am getting the following kernel related errors the while booting the uImage which is build using the latest OMAP35x Linux PSP 02.01.01.08 2.6.29-rc3 kernel source.
I had used the toolchain arm-none-linux-gnueabi-gcc-4.2.3 (arm-2008q1) which is suggested by TI for building new released dvsdk software.
Can anybody suggests me to solve this kernel panic sync error
Texas Instruments X-Loader 1.41
Starting OS Bootloader...
U-Boot 1.1.4 (Oct 17 2008 - 18:12:55)
OMAP3-GP rev 2, CPU-OPP2 L3-165MHz
OMAP3EVM 1.0 Version + mPOP (Boot NAND)
DRAM: 128 MB
NAND:256 MiB
Reading data from 0x25f800 -- 100% complete.
In: serial
Out: serial
Err: serial
Reseting CHIP... Done
LAN9x18 (0x01150002) detected.
Setting mac address: 00:50:c2:7e:89:1f
start Auto negotiation... (take ~2sec)
Auto negotiation complete, 100BaseTX, full duplex
Hit any key to stop autoboot: 0
Reseting CHIP... Done
LAN9x18 (0x01150002) detected.
Setting mac address: 00:50:c2:7e:89:1f
start Auto negotiation... (take ~2sec)
Auto negotiation complete, 100BaseTX, full duplex
TFTP from server 10.19.39.41; our IP address is 10.19.39.100
Filename 'uImage'.
Load address: 0x80000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################
done
Bytes transferred = 2082576 (1fc710 hex)
## Booting image at 80000000 ...
Image Name: Linux-2.6.29-rc3-omap1
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2082512 Bytes = 2 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
OK
Starting kernel ...
Uncompressing Linux....................................................................................................................................... done, booting the kern
el.
<5>Linux version 2.6.29-rc3-omap1 (kumarhp@localhost.localdomain) (gcc version 4.2.3 (Sourcery G++ Lite 2008q1-126)) #4 Thu Jul 9 13:52:41 IST 2009
CPU: ARMv7 Processor [411fc082] revision 2 (ARMv7), cr=10c5387f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: OMAP3 EVM
Memory policy: ECC disabled, Data cache writeback
<7>On node 0 totalpages: 22528
<7>free_area_init_node: node 0, pgdat c0424b24, node_mem_map c0448000
<7> Normal zone: 176 pages used for memmap
<7> Normal zone: 0 pages reserved
<7> Normal zone: 22352 pages, LIFO batch:3
<6>OMAP3530 ES2.1 (full speed SGX, IVA2)
<6>SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 22352
<5>Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=10.19.39.100 root=/dev/nfs nfsroot=10.19.39.41:/home/kumarhp/workdir/filesys,nolock mem=88M video=omap24xxfb:rotati
on=90
<6>Clocking rate (Crystal/DPLL/ARM core): 26.0/332/500 MHz
<6>Reprogramming SDRC
<6>GPMC revision 5.0
<6>IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts
<6>Total of 96 interrupts on 1 active controller
<6>OMAP34xx GPIO hardware version 2.5
PID hash table entries: 512 (order: 9, 2048 bytes)
<6>OMAP clockevent source: GPTIMER1 at 32768 Hz
Console: colour dummy device 80x30
<6>Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
<6>Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
<6>Memory: 88MB = 88MB total
<5>Memory: 84856KB available (3828K code, 360K data, 152K init)
<6>Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)
Mount-cache hash table entries: 512
<6>CPU: Testing write buffer coherency: ok
<6>net_namespace: 520 bytes
<6>NET: Registered protocol family 16
<4>MUX: setup J21_34XX_I2C1_SDA (0xd80021bc): 0x1718 -> 0x0118
<4>MUX: setup K21_34XX_I2C1_SCL (0xd80021ba): 0x1718 -> 0x0118
<4>MUX: setup AE15_34XX_I2C2_SDA (0xd80021c0): 0x1718 -> 0x0118
<4>MUX: setup AF15_34XX_I2C2_SCL (0xd80021be): 0x1718 -> 0x0118
<4>MUX: setup AG14_34XX_I2C3_SDA (0xd80021c4): 0x1718 -> 0x0118
<4>MUX: setup AF14_34XX_I2C3_SCL (0xd80021c2): 0x1718 -> 0x0118
<4>MUX: setup AF26_34XX_GPIO0 (0xd80021e0): 0x1718 -> 0x0118
<4>MUX: setup L8_34XX_GPIO63 (0xd80020ce): 0x1718 -> 0x0004
<4>MUX: setup AA10_3430_USB2HS_PHY_STP (0xd80025f2): 0x1700 -> 0x0003
<4>MUX: setup AA8_3430_USB2HS_PHY_CLK (0xd80025f0): 0x1700 -> 0x0003
<4>MUX: setup AA9_3430_USB2HS_PHY_DIR (0xd80025f4): 0x1700 -> 0x010b
<4>MUX: setup AB11_3430_USB2HS_PHY_NXT (0xd80025f6): 0x1700 -> 0x010b
<4>MUX: setup AB10_3430_USB2HS_PHY_D0 (0xd80025f8): 0x1700 -> 0x010b
<4>MUX: setup AB9_3430_USB2HS_PHY_D1 (0xd80025fa): 0x1700 -> 0x010b
<4>MUX: setup W3_3430_USB2HS_PHY_D2 (0xd80021d4): 0x1708 -> 0x010b
<4>MUX: setup T4_3430_USB2HS_PHY_D3 (0xd80021de): 0x1708 -> 0x010b
<4>MUX: setup T3_3430_USB2HS_PHY_D4 (0xd80021d8): 0x1700 -> 0x010b
<4>MUX: setup R3_3430_USB2HS_PHY_D5 (0xd80021da): 0x1700 -> 0x010b
<4>MUX: setup R4_3430_USB2HS_PHY_D6 (0xd80021dc): 0x1708 -> 0x010b
<4>MUX: setup T2_3430_USB2HS_PHY_D7 (0xd80021d6): 0x1700 -> 0x010b
<3>twl4030: client 2 is not initialized
<3>twl4030: client 2 is not initialized
<3>twl4030: client 2 is not initialized
<6>OMAP DMA hardware revision 4.0
<3>USB: No board-specific platform config found
<6>OMAP DSS rev 2.0
<6>OMAP DISPC rev 3.0
<6>OMAP VENC rev 2
bio: create slab <bio-0> at 0
<6>i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
<6>twl4030: PIH (irq 7) chaining IRQs 368..375
<6>twl4030: power (irq 373) chaining IRQs 376..383
<6>i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
<6>i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
<5>SCSI subsystem initialized
<6>usbcore: registered new interface driver usbfs
<6>usbcore: registered new interface driver hub
<6>usbcore: registered new device driver usb
<6>musb_hdrc: version 6.0, musb-dma, host, debug=0
<1>Unhandled fault: external abort on non-linefetch (0x1028) at 0xd80ab404
Internal error: : 1028 [#1]
Modules linked in:
CPU: 0 Not tainted (2.6.29-rc3-omap1 #4)
PC is at musb_platform_init+0xa0/0x150
LR is at _omap2_clk_enable+0xac/0xec
pc : [<c001fa58>] lr : [<c003964c>] psr: 40000013
sp : c4817d50 ip : 00000001 fp : c4817d6c
r10: c001eca0 r9 : 00000000 r8 : c0410af0
r7 : 00000000 r6 : c487f8d0 r5 : c487f8d0 r4 : c03f53c8
r3 : d80ab000 r2 : 00000200 r1 : 00000000 r0 : 00000000
Flags: nZcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c5387f Table: 80004019 DAC: 00000017
Process swapper (pid: 1, stack limit = 0xc48162e0)
Stack: (0xc4817d50 to 0xc4818000)
7d40: c487f8d0 00000000 c03f8bb4 c03f8a98
7d60: c4817e44 c4817d70 c001f080 c001f9c4 c4817d9c c4817d80 c0301d74 c007856c
7d80: c03f8a28 c03f8a30 0000005c d80ab000 c03f8b38 c4817da0 c0301dd8 c0301cc4
7da0: c4817dec c4817db0 c00eda2c c0301dd4 c00ed758 c00ed630 c484dd58 c484dcf8
7dc0: c4817df0 c485c458 c4817dec 00000000 c484dcf8 c4817df0 c485c458 00000001
7de0: c4817e24 c4817df0 c00ee6c4 c00eda1c c485c458 00000000 00000000 00000001
7e00: c00edd4c c03f8a30 00000000 c03f8a74 c041bb8c c0410af0 c4817e34 c03f8a30
7e20: c03f8ab8 c041bb8c c041bb8c c0410af0 00000000 c001eca0 c4817e54 c4817e48
7e40: c01ba530 c001ee58 c4817e74 c4817e58 c01b9744 c01ba51c c03f8a30 c03f8ab8
7e60: c041bb8c c041bb8c c4817e94 c4817e78 c01b9858 c01b967c 00000000 c4817e98
7e80: c01b97f0 c041bb8c c4817ebc c4817e98 c01b8b88 c01b97fc c48034d8 c03f8a60
7ea0: 00000000 c041bb8c c0425280 c48d0960 c4817ecc c4817ec0 c01b9588 c01b8b48
7ec0: c4817efc c4817ed0 c01b9154 c01b9574 c031a764 c041bb8c c0425280 c00268b4
7ee0: c041bb8c c0425280 00000000 00000000 c4817f24 c4817f00 c01b9a4c c01b90b8
7f00: c00268b4 c041bb70 c0425280 00000000 00000000 c001eca0 c4817f34 c4817f28
7f20: c01ba954 c01b99c0 c4817f4c c4817f38 c01ba988 c01ba8f4 c00268b4 c00267cc
7f40: c4817f5c c4817f50 c001ecdc c01ba97c c4817fdc c4817f60 c002e2b0 c001ecac
7f60: 0000015f c042fc34 c4817f94 c4817f78 c00e7c00 c00e7a18 c4817f94 c483e6e0
7f80: c00e7db0 c4817f9e c4817fc4 c4817f98 c0082d3c c00e7c3c c4817fb4 35332f18
7fa0: 00000031 00000000 00000180 c00267cc 00000000 c00268b4 c00267cc 00000000
7fc0: 00000000 00000000 00000000 00000000 c4817ff4 c4817fe0 c00088b8 c002e264
7fe0: 00000000 00000000 00000000 c4817ff8 c005dda8 c0008854 0073fe09 82f7df60
Backtrace:
[<c001f9b8>] (musb_platform_init+0x0/0x150) from [<c001f080>] (musb_probe+0x234/0xb6c)
r5:c03f8a98 r4:c03f8bb4
[<c001ee4c>] (musb_probe+0x0/0xb6c) from [<c01ba530>] (platform_drv_probe+0x20/0x24)
[<c01ba510>] (platform_drv_probe+0x0/0x24) from [<c01b9744>] (driver_probe_device+0xd4/0x180)
[<c01b9670>] (driver_probe_device+0x0/0x180) from [<c01b9858>] (__driver_attach+0x68/0x8c)
r7:c041bb8c r6:c041bb8c r5:c03f8ab8 r4:c03f8a30
[<c01b97f0>] (__driver_attach+0x0/0x8c) from [<c01b8b88>] (bus_for_each_dev+0x4c/0x84)
r7:c041bb8c r6:c01b97f0 r5:c4817e98 r4:00000000
[<c01b8b3c>] (bus_for_each_dev+0x0/0x84) from [<c01b9588>] (driver_attach+0x20/0x28)
r7:c48d0960 r6:c0425280 r5:c041bb8c r4:00000000
[<c01b9568>] (driver_attach+0x0/0x28) from [<c01b9154>] (bus_add_driver+0xa8/0x214)
[<c01b90ac>] (bus_add_driver+0x0/0x214) from [<c01b9a4c>] (driver_register+0x98/0x120)
r8:00000000 r7:00000000 r6:c0425280 r5:c041bb8c r4:c00268b4
[<c01b99b4>] (driver_register+0x0/0x120) from [<c01ba954>] (platform_driver_register+0x6c/0x88)
[<c01ba8e8>] (platform_driver_register+0x0/0x88) from [<c01ba988>] (platform_driver_probe+0x18/0x68)
[<c01ba970>] (platform_driver_probe+0x0/0x68) from [<c001ecdc>] (musb_init+0x3c/0x54)
r5:c00267cc r4:c00268b4
[<c001eca0>] (musb_init+0x0/0x54) from [<c002e2b0>] (do_one_initcall+0x58/0x184)
[<c002e258>] (do_one_initcall+0x0/0x184) from [<c00088b8>] (kernel_init+0x70/0xdc)
[<c0008848>] (kernel_init+0x0/0xdc) from [<c005dda8>] (do_exit+0x0/0x65c)
r5:00000000 r4:00000000
Code: e12fff33 ea000000 eb007f6c e59f3098 (e5932404)
<4>---[ end trace 1b75b31a2719ed1c ]---
<0>Kernel panic - not syncing: Attempted to kill init!