Hi,
when I use eg. EMIF A for NAND-Flash or MMC/SD card, I don't need all signals of the peripheral, can I use them as GPIOs then (eg. the EMIFA address lines)?
The user's guide of the McASP states so (2.3.6), but in most of the other peripheral UGs there is no specific info referring to unused signals/pins.
What makes me suspicious is this passus from the L137 datasheet: "Note that the input from each pin is always routed to all of the peripherals that share the pin; the PINMUX registers have no effect on input from a pin."
So: could it happen that an unused pin (e.g. wait or enable signals) of an activated peripheral which is configured as GPIO interfers with the function of the peripheral?
Stefan