Other Parts Discussed in Thread: DM8107
hi TI-friends,
we use giga PHY in our dm816x board and connect two boards directly. we use iperf to confirm the network speed and found the maximum speed is 600~700 Mbps which is far from 1 Gbps. We use the same tool in other arm based platform and got 800~900 Mbps. The PHY was used commonly in PC/NB product. I disable all applications after boot up and turn on this tool only...
Did you have any idea about this?? Or what can I test for your reference?