This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm following the procedure in http://processors.wiki.ti.com/index.php/AM335x_DDR_PHY_register_configuration_for_DDR3
Get stuck in below step:
"3. Connect the board to Code Composer and run the GEL file Scripts->AM335x System Initialization. Load the DDR3_slave_ratio_search_auto.out file from above and run the code. The console window in CCS will prompt you for some input values."
I cannot see any prompt after running this .out file, no where to let me input values...the gel file I use is AM335x_15x15_EVM_v1.5.gel, no error shown.
What I can do now?
Thanks,
Susan
Files needed for this procedure:
Code Composer GEL file: You can use the AM3358 StarterKit GEL to start with.
Executable CCS .out file: Media:DDR3_slave_ratio_search_auto.zip
Have you tried the StarterKit GEL?
Hi BIser,
YES I've been using the Media:DDR3_slave_ratio_search_auto.zip all the time.
When I use the AM3358 StarterKit GEL with our AM3352 board there'll show error: AM335x_EVM_Initialization() cannot be evaluated...
When I use the AM3358 StarterKit GEL with TI AM335x GM EVM board, there isn't anything show up to ask me for any parameters.
Please help on this.
Thanks,
Susan