This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I want to control a multiplexer using my TMS320C6748 DSP and the CCSv5, is it possible? How can I do it? Can I control the voltage from the logic outputs?
Thanks in advance,
Miguel.
Hi,
These are the two mux that I want to control:
http://pdf.datasheetcatalog.com/datasheets/185/420758_DS.pdf
http://www.analog.com/static/imported-files/data_sheets/ADG1604.pdf
Regards,
Miguel.
Hi,
A solution to this problem involves selecting the port you want to use on the DSP (most probably GPIO) and how to do the hardware connection to the MUXes you are using (none of them are from TI), but one thing is sure: these two details are far from being related to the CCS category.
Therefore, I strongly suggest you to ask this in the DSP forum. When asking there, make sure you send them a hardware diagram of what you plan to achieve.
--Cheers
I just want to use the mux to switch between different input and output audio signals.
As per 176671's suggestion, I will move this thread into the appropriate device forum.
Thanks
ki