Hello, I understand that a Starterware porting project with full support for the Beaglebone Black was launched last October or thereabouts. We are prototyping on a avionics product and are developing our own OS for the BeagleBone Black. After installing the BBB patch in Starterware we have been able to build and run Starterware code on the Black, but since currently we are only using a patch from the original Beaglebone code,, it does not have support for HDMI which is crucial to our development project using the BBB and bare metal OS's.
Is there any estimation when the full Starterware support for the BBB will become available? Or is there any beta HDMI driver code etc that can be obtained? Right now the emphasis is on HDMI support, but we will want full functionality of the board.
Can you provide any help?
Regards,