Hi,
I have a Beaglebone Rev. A6a with TI Sitara OS installed.
The OS installed is the last downloaded from the site AM335xSDK 07_00_00_00.
I want to connect to my beaglebone with SSL.
I have added to the file lighttpd.conf the following rows:
$SERVER["socket"] == "192.168.0.1:443" {
server.document-root = "/www/pages/"
ssl.engine = "enable"
ssl.pemfile = "/etc/lighttpd/ssl/start_page/server.pem"
}
When I restart the lighttpd I receive the following message:
root@am335x-evm:/etc# lighttpd -f lighttpd.conf
2014-03-25 09:25:34: (network.c.400) SSL: ssl requested but openssl support is not compiled in
Can anyone help me about this problem?