All:
Using instructions in SPRUHD3G "TI RTOS 1.21 Getting Started Guide" I have been able to make some progress on using TI-RTOS with F5529. However, I have some feedback and a question.
1. It would seem that TI could provide a workspace and project files for the examples. I have had to create both to get a relatively simple example to get going.
2. The tirtos and xdc support files needed to be copied into the c:\ti directory for "Configure Custom Argument Variables" of section 3.3.2 of the Getting Started Guide. If not, I was unable to make progress.
3. I needed to physically point to the xdc\include directory in the c:\ti directory. This took a little bit of time to even find. [C:\ti\xdctools_3_30_01_25_core\packages\xdc\platform\package ]
4. Once I did this, I was not able to see the nice list of TI examples showni in the figure of section 3.3.3, step 9 - instead, I had to physcially port the files needed. (I am using the GPIO example first.)
5. Under the options for "IARdemo" (section 3.3.3 step 10), I also needed to specify the processor under General Options.
When I build, I get an error that I need help with. I get pointed to a std.h file with the following line as an error:
* 'xdc_target_types__' must be defined to name a target-specific header
* file (e.g., ti/targets/std.h) that has definitions for the basic types:
* xdc_Int8, xdc_Int16, ...
*
* For example, to build for a target in the ti.targets package you should
* add the following option to your compiler's command line:
* -Dxdc_target_types__=ti/targets/std.h
*/
#error xdc_target_types__ must be defined to name a target-specific header containing definitions of xdc_Int8, xdc_Int16, ...
Can someone tell me how to add the info required?