We are using a custom AM437x board with the same PMIC as the AM437x GP EVM. Sometimes our board shuts down after 20 seconds. We have not been able to find a pattern for when it shuts down, it's very random. I have narrowed down the problem to the PMIC PWR_EN signal coming from the RTC_PMIC_EN (AD6) pin on the AM437x. This should always be outputting logic high so the PMIC stays on, but occasionally it does not. If we tie that signal to a 1.8V supply, the board remains on. Is there some way to solve this issue?
Thanks,
Trent