hi all
I want to Upgrading the U_Boot of the DVEVM-DM6446,
so I according to dvsdk_2_00_00_22/PSP_02_00_00_140/docs/commands.txt
this is my steps on uboot
#setenv serverip 192.168.0.12
#setenv ipaddr 192.168.0.15
#tftp 0x80700000 u-boot-1.2.0-davinci-nand.bin
#nand erase 0x18000 0x20000
#nand write 0x80700000 0x18000 0x20000
then I boot the kernel
# boot
this all right!!
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
When I DVEVM power outage, and again on the power, it prompts me the following:
(S3 set [1...10]:0000111110,J4 jump NAND)
DM644x initialization passed!
TI UBL Version: 1.50
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
No valid boot image found!
NAND Boot failed.
Aborting...
(stop.......)
then how can I do thanks!
by the way my dvevm dm6446 nand flash is 64M but the commands.txt say 32M,what wrong?
How do I do to upgrade my uboot ?
thank you !!