Hello E2E members and TI employees.
I have a question related to hyperlink test externally on two 66AK2H12 with RTM-BOC.
Test environment is as follows.
(1) target: two 66AK2H12 with RTM-BOC (refer to below picture)
(2) example project name: hyplnk_K2HC66BiosExampleProject
(3) test method: run 'hyplnk_K2HC66BiosExampleProject.out' each target on the dsp core0.
(4) console message:
[C66xx_0] Version #: 0x02010001; string HYPLNK LLD Revision: 02.01.00.01:Oct 1 2014:23:55:00
About to do system setup (PLL, PSC, and DDR)
Constructed SERDES configs: PLL=0x00000228; RX=0x0046c485; TX=0x000cc305
system setup worked
About to set up HyperLink Peripheral
============================Hyperlink Testing Port 0
========================================== begin registers before initialization ===========
Revision register contents:
Raw = 0x4e902101
Status register contents:
Raw = 0x00003004
Link status register contents:
Raw = 0x00000000
Control register contents:
Raw = 0x00000000
Control register contents:
Raw = 0x00000000
============== end registers before initialization ===========
Waiting for other side to come up ( 0)
Waiting for other side to come up ( 1)
Waiting for other side to come up ( 2)
...
I think that the example code is not suitable completely for keystone II devices, and that needs to modify some codes for this test.
If you have a comment to solve about that, please tell me how to solve it.
Thank you!
Gilbert Kim.