hello all ;
Something is wrong with my Linux 3.4.8 on EVMK2h . and i want to restore it using u-boot prompt .
so is it possible or not ? if yes please how ?
thank you .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello all ;
Something is wrong with my Linux 3.4.8 on EVMK2h . and i want to restore it using u-boot prompt .
so is it possible or not ? if yes please how ?
thank you .
Hi Capitaine,
Yes it is possible to put a linux kernel image using u-boot prompt using tftpboot method.
Being in the u-boot prompt, you will use the command like below.
For K2H:-
>tftpboot 0x87000000 uImage-k2hk-evm.dtb
>tftpboot 0x88000000 uImage-keystone-evm.bin
>tftpboot 0x0c5f0000 skern-k2hk.bin
>mon_install 0x0c5f0000
>bootm 0x88000000 - 0x87000000
For more information please visit : http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Exploring#Trouble_shooting_and_FAQ
Regards,
Shankari
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------