This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730 cvbs out port problems



I have a mistral EVM, the revisions are , main board REV G, proc board REV D.

I have tested the cvbs in and out with the program located in ti-dvsdk_dm3730-evm_4_02_00_06\dmai_2_20_00_15\packages\ti\sdo\dmai\apps,

Following problems found:

1.No matter a NTSC or Pal signal is fed to the board, board cannot provide a NTSC output,  only PAL signal are output to TV.

2. No matter a NTSC or PAL signal is captured, There is only Y component can be seen on TV , without Cb, Cr.  While, if used LCD instead of cvbs, everything looks well.

hope you technical help.