Sequence ID: 0
Error Code: -1063
Error Class: 0x80000200
I/O Port = 378
Board Name: C671x PP Emulator
Cpu Name: cpu_0
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tran,
What target configuration you have done?
I am using ccs5.5 and its working fine for me.
Try with this configuration, also do test connection
Check below mentioned thread, it may help you out.
Hi Tran,
Have you tried to connect your XDS510USB emulator with some other board, if not then try it.
For me it's working fine.
My environment setup is- CCSv5.5
Switch Setting(SW3) - HPI/Emulation boot
pin 1 | off |
pin 2 | off |
pin 3 | on |
pin 4 | off |
After going for test connection , it gives below mentioned output
You can try to debug jtag connection also , refer this link
http://processors.wiki.ti.com/index.php/Debugging_JTAG_Connectivity_Problems