This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a board with a DDR layout almost identical to BeagleBoneBlack.
The board seems to run fine with the default BBB DDR3 settings, but when trying to tune the values I get odd "optimum" values from the tool.
I have followed the instructions here:
using the specified BBB gel file.
Inputs to the seed tool are:
PHY_INVERT_CLKOUT 0
Seed values used in CCS code
DATAx_PHY_RD DQS_SLAVE_RATIO 40
DATAx_PHY_FIFO_WE_SLAVE_RATIO 75
DATAx_PHY_WR DQS_SLAVE_RATIO 2
Register value
CMDx_PHY_CTRL_SLAVE_RATIO 80
Running the tool to tune the settings ends up with the following:
***************************************************************
The Slave Ratio Search Program Values are...
***************************************************************
PARAMETER MAX | MIN | OPTIMUM | RANGE
***************************************************************
DATA_PHY_RD_DQS_SLAVE_RATIO 0x3ff | 0x0bb | 0x25d | 0x344
DATA_PHY_FIFO_WE_SLAVE_RATIO 0x3ff | 0x000 | 0x1ff | 0x3ff
DATA_PHY_WR_DQS_SLAVE_RATIO 0x07a | 0x000 | 0x03d | 0x07a
DATA_PHY_WR_DATA_SLAVE_RATIO 0x3ff | 0x03c | 0x21d | 0x3c3
***************************************************************
===== END OF TEST =====
When using these values, u-boot then fails to start.
Any idea on why these values are so different from what a BBB generates?
I am running CCS Version: 6.1.0.00104
Hi,
Can you post your Ratio Seed Excel sheet?
Everything seems correct here. I will ask the DDR experts to look at this.
Aside from this, posting a file is easy - just drag and drop it in your reply window.
Ok, problem seems to be found, my board was running off a 25MHz crystal and the gel-file was only setup for BBB which uses 24MHz.
There was an error message thrown, but the script did not terminate so I did not see it.
Once I added the 25MHz config, I got relevant numbers and also the EDMA test passes.
So for others using this software, be aware of the configuration if you do not use 24MHz
I only have a 800MHz version of the processor, so I can not run at 1GHz, but here is the section that I use to configure the PLLs:
In the 'hotmenu ARM_OPP100_Config()' section I added this code:
else if(CLKIN==25)
{
MPU_PLL_Config( CLKIN, 24, 500, 1);
CORE_PLL_Config( CLKIN, 24, 500, 10, 8, 4);
// DDR3 400MHz setting
// DDR_PLL_Config( CLKIN, 24, 400, 1);
// DDR3 303MHz setting
GEL_TextOut("**** Setting DDR PLL to 303MHz ......... \n","Output",1,1,1);
DDR_PLL_Config( CLKIN, 24, 303, 1);
PER_PLL_Config( CLKIN, 24, 960, 5);
DISP_PLL_Config( CLKIN, 24, 48, 1);
GEL_TextOut("**** AM335x ALL ADPLL Config for OPP == OPP100, 25MHz input is Done ......... \n","Output",1,1,1);
}
/PA