This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x GPMC device tree configuration for SRAM access

Hi

I need to configure a device tree (dts) for AM335x ( BeagleBone Black ) GPMC to access a 16 bits data, 1Mbytes SRAM ( Static RAM memory ), with NO multiplexed address with data. Where can I find information about device tree codification for this GPMC configuration?

Thank you

Sergio

  • Hi Sergio,

    I am not aware of a TI example code for this specific use case.

    However you can see what each of the parameters in the GPMC dts nodes is used for in Documentation/devicetree/bindings/memory-controller/omap-gpmc.txt (I am attaching the file here: 

    Device tree bindings for OMAP general purpose memory controllers (GPMC)
    
    The actual devices are instantiated from the child nodes of a GPMC node.
    
    Required properties:
    
     - compatible:		Should be set to one of the following:
    
    			ti,omap2420-gpmc (omap2420)
    			ti,omap2430-gpmc (omap2430)
    			ti,omap3430-gpmc (omap3430 & omap3630)
    			ti,omap4430-gpmc (omap4430 & omap4460 & omap543x)
    			ti,am3352-gpmc   (am335x devices)
    
     - reg:			A resource specifier for the register space
    			(see the example below)
     - ti,hwmods:		Should be set to "ti,gpmc" until the DT transition is
    			completed.
     - #address-cells:	Must be set to 2 to allow memory address translation
     - #size-cells:		Must be set to 1 to allow CS address passing
     - gpmc,num-cs:		The maximum number of chip-select lines that controller
    			can support.
     - gpmc,num-waitpins:	The maximum number of wait pins that controller can
    			support.
     - ranges:		Must be set up to reflect the memory layout with four
    			integer values for each chip-select line in use:
    
    			   <cs-number> 0 <physical address of mapping> <size>
    
    			Currently, calculated values derived from the contents
    			of the per-CS register GPMC_CONFIG7 (as set up by the
    			bootloader) are used for the physical address decoding.
    			As this will change in the future, filling correct
    			values here is a requirement.
    
    GPMC DMA information.
     - dmas			GPMC dma channel
     - dma-names		Must be set to "rxtx"
    
    Timing properties for child nodes. All are optional and default to 0.
    
     - gpmc,sync-clk-ps:	Minimum clock period for synchronous mode, in picoseconds
    
     Chip-select signal timings (in nanoseconds) corresponding to GPMC_CONFIG2:
     - gpmc,cs-on-ns:	Assertion time
     - gpmc,cs-rd-off-ns:	Read deassertion time
     - gpmc,cs-wr-off-ns:	Write deassertion time
    
     ADV signal timings (in nanoseconds) corresponding to GPMC_CONFIG3:
     - gpmc,adv-on-ns:	Assertion time
     - gpmc,adv-rd-off-ns:	Read deassertion time
     - gpmc,adv-wr-off-ns:	Write deassertion time
    
     WE signals timings (in nanoseconds) corresponding to GPMC_CONFIG4:
     - gpmc,we-on-ns	Assertion time
     - gpmc,we-off-ns:	Deassertion time
    
     OE signals timings (in nanoseconds) corresponding to GPMC_CONFIG4:
     - gpmc,oe-on-ns:	Assertion time
     - gpmc,oe-off-ns:	Deassertion time
    
     Access time and cycle time timings (in nanoseconds) corresponding to
     GPMC_CONFIG5:
     - gpmc,page-burst-access-ns: 	Multiple access word delay
     - gpmc,access-ns:		Start-cycle to first data valid delay
     - gpmc,rd-cycle-ns:		Total read cycle time
     - gpmc,wr-cycle-ns:		Total write cycle time
     - gpmc,bus-turnaround-ns:	Turn-around time between successive accesses
     - gpmc,cycle2cycle-delay-ns:	Delay between chip-select pulses
     - gpmc,clk-activation-ns: 	GPMC clock activation time
     - gpmc,wait-monitoring-ns:	Start of wait monitoring with regard to valid
    				data
    
    Boolean timing parameters. If property is present parameter enabled and
    disabled if omitted:
     - gpmc,adv-extra-delay:	ADV signal is delayed by half GPMC clock
     - gpmc,cs-extra-delay:		CS signal is delayed by half GPMC clock
     - gpmc,cycle2cycle-diffcsen:	Add "cycle2cycle-delay" between successive
    				accesses to a different CS
     - gpmc,cycle2cycle-samecsen:	Add "cycle2cycle-delay" between successive
    				accesses to the same CS
     - gpmc,oe-extra-delay:		OE signal is delayed by half GPMC clock
     - gpmc,we-extra-delay:		WE signal is delayed by half GPMC clock
     - gpmc,time-para-granularity:	Multiply all access times by 2
    
    The following are only applicable to OMAP3+ and AM335x:
     - gpmc,wr-access-ns:		In synchronous write mode, for single or
    				burst accesses, defines the number of
    				GPMC_FCLK cycles from start access time
    				to the GPMC_CLK rising edge used by the
    				memory device for the first data capture.
     - gpmc,wr-data-mux-bus-ns:	In address-data multiplex mode, specifies
    				the time when the first data is driven on
    				the address-data bus.
    
    GPMC chip-select settings properties for child nodes. All are optional.
    
    - gpmc,burst-length	Page/burst length. Must be 4, 8 or 16.
    - gpmc,burst-wrap	Enables wrap bursting
    - gpmc,burst-read	Enables read page/burst mode
    - gpmc,burst-write	Enables write page/burst mode
    - gpmc,device-width	Total width of device(s) connected to a GPMC
    			chip-select in bytes. The GPMC supports 8-bit
    			and 16-bit devices and so this property must be
    			1 or 2.
    - gpmc,mux-add-data	Address and data multiplexing configuration.
    			Valid values are 1 for address-address-data
    			multiplexing mode and 2 for address-data
    			multiplexing mode.
    - gpmc,sync-read	Enables synchronous read. Defaults to asynchronous
    			is this is not set.
    - gpmc,sync-write	Enables synchronous writes. Defaults to asynchronous
    			is this is not set.
    - gpmc,wait-pin		Wait-pin used by client. Must be less than
    			"gpmc,num-waitpins".
    - gpmc,wait-on-read	Enables wait monitoring on reads.
    - gpmc,wait-on-write	Enables wait monitoring on writes.
    
    Example for an AM33xx board:
    
    	gpmc: gpmc@50000000 {
    		compatible = "ti,am3352-gpmc";
    		ti,hwmods = "gpmc";
    		reg = <0x50000000 0x2000>;
    		interrupts = <100>;
    		dmas = <&edma 52>;
    		dma-names = "rxtx";
    		gpmc,num-cs = <8>;
    		gpmc,num-waitpins = <2>;
    		#address-cells = <2>;
    		#size-cells = <1>;
    		ranges = <0 0 0x08000000 0x10000000>; /* CS0 @addr 0x8000000, size 0x10000000 */
    
    		/* child nodes go here */
    	};
    

    You can use this example as a reference to create your custom dts node. 

    There is a gpmc-nor.txt & gpmc-nand.txt examples as well. They are located in Documentation/devicetree/bindings/mtd/

    Also, if you search for GPMC in this forum, you will find plenty of discussions, which will be of use to you, like: 
      

    Hope this helps. 

    Best Regards, 

    Yordan

  • Hi Yordan

    I read your post of Fri,May 15 2015 7:28AM about dts for SRAM that you answered to Marina and have some questions about:

    sram{
    reg = <1 0 0x01000000>; /*CSn1*/

    bank-width = <2>; /* GPMC_CONFIG1_DEVICESIZE(1) */

    /*gpmc,burst-write;*/
    /*gpmc,burst-read;*/
    /*gpmc,burst-wrap;*/
    gpmc,sync-read; /* GPMC_CONFIG1_READTYPE_ASYNC */
    gpmc,sync-write; /* GPMC_CONFIG1_WRITETYPE_ASYNC */
    gpmc,clk-activation-ns = <0>; /* GPMC_CONFIG1_CLKACTIVATIONTIME(2) */
    gpmc,burst-length = <16>; /* GPMC_CONFIG1_PAGE_LEN(2) */
    gpmc,mux-add-data = <2>; /* GPMC_CONFIG1_MUXTYPE(2) */

    gpmc,sync-clk-ps = <20000>; /* CONFIG2 */

    gpmc,cs-on-ns = <0>;
    gpmc,cs-rd-off-ns = <100>;
    gpmc,cs-wr-off-ns = <40>;

    gpmc,adv-on-ns = <0>; /* CONFIG3 */
    gpmc,adv-rd-off-ns = <20>;
    gpmc,adv-wr-off-ns = <20>;

    gpmc,we-on-ns = <20>; /* CONFIG4 */
    gpmc,we-off-ns = <40>;
    gpmc,oe-on-ns = <20>;
    gpmc,oe-off-ns = <100>;

    gpmc,page-burst-access-ns = <20>; /* CONFIG 5 */
    gpmc,access-ns = <80>;
    gpmc,rd-cycle-ns = <120>;
    gpmc,wr-cycle-ns = <60>;
    gpmc,wr-access-ns = <40>; /* CONFIG 6 */
    gpmc,wr-data-mux-bus-ns = <20>;

    /*gpmc,bus-turnaround-ns = <40>;*/ /* CONFIG6:3:0 = 4 */
    gpmc,cycle2cycle-samecsen; /* CONFIG6:7 = 1 */
    gpmc,cycle2cycle-delay-ns = <20>; /* CONFIG6:11:8 = 4 */

    /* not using dma engine yet, but we can get the channel number here */

    };

    Question 1:

    /*gpmc,burst-write;*/
    /*gpmc,burst-read;*/
    /*gpmc,burst-wrap;*/
    These 3 lines commented, means that GPMC will not use burst access?
    If so, then the following line can be commented also, that is right?
    gpmc,page-burst-access-ns = <20>; /* CONFIG 5 */


    Question 2:

    gpmc,cs-rd-off-ns = <100>;
    This declaration means that the time to cs-rd-off-ns will be 100 ns?


    Question 3:

    How to declare that GPMC must not multiplex address with data?
    I need a GPMC configuration that will not multiplex address with data.
    The absence of address/data mux declaration implies that GPMC will not multiplex address/data?


    Excuse me for being so primary in these questions, but, the fact is, I am in the middle of a video grabber cape board for BeagleBone Black development and I need to be sure about these configurations.

    Thank you very much Yordan.

    Sergio
  • Hi Sergio,

    Sorry for the delayed response.
    Question1:
    " - gpmc,burst-wrap Enables wrap bursting
    - gpmc,burst-read Enables read page/burst mode
    - gpmc,burst-write Enables write page/burst mode"
    So yes, commenting these lines will disable the burst access. You CAN comment gpmc,page-burst-access-ns = <20>; /* CONFIG 5 */ as well.

    Question2:
    Here is the explanation for CS Timings:
    " Chip-select signal timings (in nanoseconds) corresponding to GPMC_CONFIG2:
    - gpmc,cs-on-ns: Assertion time
    - gpmc,cs-rd-off-ns: Read deassertion time
    - gpmc,cs-wr-off-ns: Write deassertion time"

    Question 3:
    The gpmc,mux-add-data ENABLES this GPMC feature:
    "gpmc,mux-add-data Address and data multiplexing configuration.
    Valid values are 1 for address-address-data
    multiplexing mode and 2 for address-data
    multiplexing mode. "

    So if the gpmc,mux-add-data is not declared in the GPMC dts node, then the driver won't enable address and data multiplexing

    FYI, all of this info is available in kernel documentation: Documentation/devicetree/bindings/memory-controllers/omap-gpmc.txt

    Best Regards,
    Yordan
  • Hi Yordan

    Thank you for your kind support.

    The GPMC interface is working fine now as SRAM interface.

    Two more questions please:

    - As GPMC does not multiplex address with data, in the SRAM configuration ( address/data multiplexing consumes time ), I am understanding that this NOMUX ( parallel address/data) configuration is FASTER than any other MUX configuration (assuming not using bursting), is that right?

    - On the other hand, due SRAM characteristics ( address and data in parallel mode ), I can't use BURST MODE in SRAM access, is that right?

    The reason for these questions is that I am searching for the faster way to access my device, because, as a matter of fact, it is not a SRAM ( Static RAM ), but, a video frame FIFO ( sequential memory ), and I need only the RD, OE and CS1 ( and of course, the 16 bit DATA bus ), where all address lines are discarded.

    Sergio
  • Hi Sergio,

    Correct, my understanding is the same.

    Best Regards,
    Yordan
  • Dear Yordan:

    I also need to configure a device tree (dts) for AM335x ( BeagleBone Black ) GPMC to access a 16 bits data, 1Mbytes SRAM ( Static RAM memory ), with NO multiplexed address with data.

    I applied below device tree too, linux kernel is 4.3.13.  but I can not see sram range in /proc/iomem

    &gpmc {
            status = "okay";
            pinctrl-names = "default";
            pinctrl-0 = <&gpmc_pins>;

            #address-cells = <2>;
            #size-cells = <1>;

            /* chip select ranges */
            ranges = <1 0 0x01000000 0x1000000>;

            sram{
                    reg = <1 0 0x01000000>; /*CSn1*/

                    bank-width = <2>;        /* GPMC_CONFIG1_DEVICESIZE(1) */

                    /*gpmc,burst-write;*/
                    /*gpmc,burst-read;*/
                    /*gpmc,burst-wrap;*/
                    gpmc,sync-read;  /* GPMC_CONFIG1_READTYPE_ASYNC */
       ...

     

    my iomem is as below

    root@arm:~# cat /proc/iomem
    40300000-4030ffff : 40300000.ocmcram
    44d00000-44d03fff : umem
    44d80000-44d81fff : dmem
    44e07000-44e07fff : /ocp/gpio@44e07000
    44e09000-44e0901f : serial
    44e0b000-44e0bfff : /ocp/i2c@44e0b000
    44e10620-44e1062f : phy_ctrl
    44e10648-44e1064b : wakeup
    44e10650-44e10653 : gmii-sel
    44e10800-44e10a37 : pinctrl-single
    44e35000-44e35fff : /ocp/wdt@44e35000
    44e3e000-44e3efff : /ocp/rtc@44e3e000
    47401000-474011ff : control
    47401400-474017ff : mc
      47401400-474017ff : mc
    47401800-474019ff : control
    47401c00-47401fff : mc
      47401c00-47401fff : mc
    48022000-4802201f : serial
    48024000-4802401f : serial
    48030100-480304ff : /ocp/spi@48030000
    48038000-48039fff : mpu
    4803c000-4803dfff : mpu
    48042000-480423ff : /ocp/timer@48042000
    48044000-480443ff : /ocp/timer@48044000
    48046000-480463ff : /ocp/timer@48046000
    48048000-480483ff : /ocp/timer@48048000
    4804a000-4804a3ff : /ocp/timer@4804a000
    4804c000-4804cfff : /ocp/gpio@4804c000
    48060000-48060fff : /ocp/mmc@48060000
    480c8000-480c81ff : /ocp/mailbox@480C8000
    4819c000-4819cfff : /ocp/i2c@4819c000
    481a0100-481a04ff : /ocp/spi@481a0000
    481a8000-481a801f : serial
    481aa000-481aa01f : serial
    481ac000-481acfff : /ocp/gpio@481ac000
    481ae000-481aefff : /ocp/gpio@481ae000
    48310000-48311fff : /ocp/rng@48310000
    49000000-4900ffff : /ocp/edma@49000000
    4a100000-4a1007ff : /ocp/ethernet@4a100000
    4a101000-4a1010ff : /ocp/ethernet@4a100000/mdio@4a101000
    4a101200-4a1012ff : /ocp/ethernet@4a100000
    50000000-50001fff : /ocp/gpmc@50000000
    53500000-5350009f : /ocp/aes@53500000
    80000000-9fffffff : System RAM
      80008000-80a39993 : Kernel code
      80aae000-80c5fb2b : Kernel data

  • Dear Sergio: Would you share me your DTS? thank you very much!
  • Hi Tsao

    Follows my DTS. Change txt to dts.

    Be aware that I am using a video FIFO, not a true SRAM, so, in practice, I don't use address bus, only data bus and control bus, but, I think that the configuration in my DTS is OK for a SRAM.

    Sergio

    /*
     * Copyright (C) 2016 WARP TECNOLOGIA ( BRAZIL )
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    /dts-v1/;
    /plugin/;
    
    / {
    	compatible = "ti,beaglebone", "ti,beaglebone-black";
    
    	/* identification */
    	part-number = "bdq9100";
    	version = "00A0","A0";
    
    	/* state the resources this cape uses */
    	exclusive-use =
    		/* the pin header uses */
    		"P8.25",	/* gpmc: gpmc_ad0 */
    		"P8.24",	/* gpmc: gpmc_ad1 */
    		"P8.5",		/* gpmc: gpmc_ad2 */
    		"P8.6",		/* gpmc: gpmc_ad3 */
    		"P8.23",	/* gpmc: gpmc_ad4 */
    		"P8.22",	/* gpmc: gpmc_ad5 */
    		"P8.3",		/* gpmc: gpmc_ad6 */
    		"P8.4",		/* gpmc: gpmc_ad7 */
    		"P8.19",	/* gpmc: gpmc_ad8 */
    		"P8.13",	/* gpmc: gpmc_ad9 */
    		"P8.14",	/* gpmc: gpmc_ad10 */
    		"P8.17",	/* gpmc: gpmc_ad11 */
    		"P8.12",	/* gpmc: gpmc_ad12 */
    		"P8.11",	/* gpmc: gpmc_ad13 */
    		"P8.16",	/* gpmc: gpmc_ad14 */
    		"P8.15",	/* gpmc: gpmc_ad15 */
    		"P9.13",	/* gpmc: gpmc_wpn */
    		"P8.21",	/* gpmc: gpmc_csn1 */
    		"P8.18",	/* gpmc: gpmc_clk */
    		"P8.7",		/* gpmc: gpmc_advn_ale */
    		"P8.8",		/* gpmc: gpmc_oen_ren */
    		"P8.10",	/* gpmc: gpmc_wen */
    		"P8.9",		/* gpmc: gpmc_ben0_cle */
    		"P9.41",	/* cssp: clkout2 */
    		"P9.42",	/* cssp: xdma_event_intr2 */
    		"P9.18",	/* cssp: gpio0_4 */
    		"P9.17",	/* cssp: gpio0_5 */
    		"P9.11",	/* cssp: gpio0_30 */
    /*		"P8.20",	 bdq9100: gpio1_31 */
    		"P8.26",	/* bdq9100: gpio1_20 */
    
    		/* the hardware IP uses */
    		"gpio0_4", 
    		"gpio0_5", 
    		"gpio0_30", 
    		"gpmc",
    		"clkout2",
    		"gpio1_31",
    		"gpio1_29",
    		/* the reset pin */
    		"eMMC_RSTn";
    
    	#address-cells = <1>;
    	#size-cells = <1>;
    
    	fragment@0 {
    		target = <&am33xx_pinmux>;
    		__overlay__ {
    
    			gpmc_pins: pinmux_gpmc_pins {
    				pinctrl-single,pins = <
    					0x000 0x30	/* gpmc_ad0.gpmc_ad0 MODE0 | INPUT | PULLUP */
    					0x004 0x30	/* gpmc_ad1.gpmc_ad1 MODE0 | INPUT | PULLUP */
    					0x008 0x30	/* gpmc_ad2.gpmc_ad2 MODE0 | INPUT | PULLUP */
    					0x00C 0x30	/* gpmc_ad3.gpmc_ad3 MODE0 | INPUT | PULLUP */
    					0x010 0x30	/* gpmc_ad4.gpmc_ad4 MODE0 | INPUT | PULLUP */
    					0x014 0x30	/* gpmc_ad5.gpmc_ad5 MODE0 | INPUT | PULLUP */
    					0x018 0x30	/* gpmc_ad6.gpmc_ad6 MODE0 | INPUT | PULLUP */
    					0x01C 0x30	/* gpmc_ad7.gpmc_ad7 MODE0 | INPUT | PULLUP */
    					0x020 0x30	/* gpmc_ad8.gpmc_ad8 MODE0 | INPUT | PULLUP */
    					0x024 0x30	/* gpmc_ad9.gpmc_ad9 MODE0 | INPUT | PULLUP */
    					0x028 0x30	/* gpmc_ad10.gpmc_ad10 MODE0 | INPUT | PULLUP */
    					0x02C 0x30	/* gpmc_ad11.gpmc_ad11 MODE0 | INPUT | PULLUP */
    					0x030 0x30	/* gpmc_ad12.gpmc_ad12 MODE0 | INPUT | PULLUP */
    					0x034 0x30	/* gpmc_ad13.gpmc_ad13 MODE0 | INPUT | PULLUP */
    					0x038 0x30	/* gpmc_ad14.gpmc_ad14 MODE0 | INPUT | PULLUP */
    					0x03C 0x30	/* gpmc_ad15.gpmc_ad15 MODE0 | INPUT | PULLUP */
    					0x074 0x30	/* gpmc_wpn.gpmc_wpn MODE0 | INPUT | PULLUP */ /* WAS MODE 7 */
    					0x080 0x08	/* gpmc_cscn1.gpmc_cscn1 MODE0 | OUTPUT */
    					0x08C 0x28	/* gpmc_clk.gpmc_clk MODE0 | INPUT */
    					0x090 0x08	/* gpmc_advn_ale.gpmc_advn_ale MODE0 | OUTPUT */
    					0x094 0x08	/* gpmc_oen_ren.gpmc_oen_ren MODE0 | OUTPUT */
    					0x098 0x08	/* gpmc_wen.gpmc_wen MODE0 | OUTPUT */
    /*					0x09C 0x08	 gpmc_ben0_cle.gpmc_ben0_cle MODE0 | OUTPUT */
    				>;
    			};
    			bdq9100_config_pins: pinmux_bdq9100_camera_pins {
    				pinctrl-single,pins = <
    					/* clkout2 */
    					0x1B4 0x03	/* xdma_event_intr1.clkout2 MODE3 | OUTPUT clkout2 */
    
    					/* dmar */
    					0x164 0x2e	/* ecap0_in_pwm0_out.xdma_event_intr2 MODE6 | INPUT */
    
    					/* bdq9100 camera */
    /*					0x084 0x37	  gpio1_31 | MODE7 | INPUT | PULLUPEN */
    					0x09C 0x37	/* gpio2_5 | MODE7 | INPUT | PULLUPEN */ 
    					0x07C 0x37	/* gpio1_29 | MODE7 | INPUT | PULLUPEN */ 
    
    				>;
    			};
    		};
    	};
    
    	fragment@1 {
    		target = <&gpmc>;
    		depth = <1>;	/* only create devices on depth 1 */
    
    		#address-cells = <1>;
    		#size-cells = <1>;
    		ranges;
    
    		__overlay__ {
    
    			status = "okay";
    
    			#address-cells = <2>;
    			#size-cells = <1>;
    
    			pinctrl-names = "default";
    			pinctrl-0 = <&gpmc_pins>;
    
    			/* chip select ranges */
    			ranges = <0 0 0x08000000 0x10000000>,	/* bootloader has this enabled */
    				 <1 0 0x18000000 0x08000000>,
    				 <2 0 0x20000000 0x08000000>,
    				 <3 0 0x28000000 0x08000000>,
    				 <4 0 0x30000000 0x08000000>,
    				 <5 0 0x38000000 0x04000000>,
    				 <6 0 0x3c000000 0x04000000>;
    				 
    			camera{
    				compatible = "bdq9100";
    				status = "okay";
    				pinctrl-names = "default";
    				pinctrl-0 = <&bdq9100_config_pins>;
    
    				reg = <1 0 0x01000000>;	/*CSn1*/
    
    				bank-width = <2>;		/* GPMC_CONFIG1_DEVICESIZE(1) */
    
    				gpmc,sync-read;					/* GPMC_CONFIG1_READTYPE_ASYNC */
    				gpmc,sync-write;				/* GPMC_CONFIG1_WRITETYPE_ASYNC */
    				gpmc,clk-activation-ns = <0>;	/* GPMC_CONFIG1_CLKACTIVATIONTIME(2) */
    				gpmc,mux-add-data = <0>;		/* GPMC_CONFIG1_MUXTYPE(0) */
    
    				gpmc,sync-clk-ps = <20000>;		/* CONFIG2 */
    
    				gpmc,cs-on-ns = <0>;
    				gpmc,cs-rd-off-ns = <100>;
    				gpmc,cs-wr-off-ns = <100>;		/*<40>; */
    
    				gpmc,adv-on-ns = <0>;			/* CONFIG3 */
    				gpmc,adv-rd-off-ns = <20>;
    				gpmc,adv-wr-off-ns = <20>;
    
    				gpmc,we-on-ns = <20>;			/* CONFIG4 */
    				gpmc,we-off-ns = <40>;
    				gpmc,oe-on-ns = <20>;
    				gpmc,oe-off-ns = <100>;
    
    				gpmc,page-burst-access-ns = <20>;	/* CONFIG 5 */
    				gpmc,access-ns = <80>;
    				gpmc,rd-cycle-ns = <120>;
    				gpmc,wr-cycle-ns = <60>;
    				gpmc,wr-access-ns = <40>;		/* CONFIG 6 */
    				gpmc,wr-data-mux-bus-ns = <20>;
    
    
    				/* dma channel */
    				dmas = <&edma 20>;
    				dma-names = "bdq";
    
    				/* tw9910 video decoder */
    				bdq-9100,decoder {
    					i2c-adapter = <&i2c2>;
    
    					/* need it to stop the whinning */
    					#address-cells = <1>;
    					#size-cells = <0>;
    
    					/* fake i2c device node */
    					fake_tw9910 {
    						compatible = "techwell,tw9910";
    						reg = <0x44>;
    						
    						/* buswidth e MPOUT */
    						buswidth = <16>;	/* TW9910 em 16 bits */
    						mpout = <6>;		/* MPOUT como FIELD */
    					};
    				};
    
    			};
    
    		};
    	};
    
    };