Other Parts Discussed in Thread: TCA9554, PCF8574, TPS65910, TLV320AIC3106
Hi,
I work on Sitara am335x-evmsk base on ti-processor-sdk-linux-am335x-evm-02.00.00.00 os.
the problem is that 48060000.mmc cd is not send an interrupt when the sd card are get out and in to cd base.
here is how mmc1 define in the DTS:
mmc1_pins_default: pinmux_mmc1_pins {
pinctrl-single,pins = <
0x0F0 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat3.mmc0_dat3 */
0x0F4 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat2.mmc0_dat2 */
0x0F8 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat1.mmc0_dat1 */
0x0FC (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat0.mmc0_dat0 */
0x100 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_clk.mmc0_clk */
0x104 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_cmd.mmc0_cmd */
0x1A0 (PIN_INPUT_PULLUP | MUX_MODE7) /* mcasp0_aclkr.gpio3_18 */
0x160 (PIN_INPUT | MUX_MODE7) /* spi0_cs1.gpio0_6 */
>;
};
mmc1_pins_sleep: pinmux_mmc1_pins_sleep {
pinctrl-single,pins = <
0x0F0 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x0F4 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x0F8 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x0FC (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x100 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x104 (PIN_INPUT_PULLDOWN | MUX_MODE7)
//0x1A0 (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
&mmc1 {
status = "okay";
vmmc-supply = <&vmmc_reg>;
bus-width = <4>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&mmc1_pins_default>;
pinctrl-1 = <&mmc1_pins_sleep>;
cd-gpios = <&gpio2 1 GPIO_ACTIVE_HIGH>;
};
the result of "cat /proc/interrupts" is:
root@am335x-evm:~# cat /proc/interrupts
CPU0
16: 5148 INTC 68 Level gp_timer
19: 1 INTC 78 Level wkup_m3_txev
20: 3333 INTC 12 Level edma
22: 26 INTC 14 Level edma_error
61: 0 4804c000.gpio 4 Edge button4
91: 0 481ac000.gpio 1 Edge 48060000.mmc cd
92: 0 481ac000.gpio 2 Edge button2
93: 0 481ac000.gpio 3 Edge button1
94: 0 481ac000.gpio 4 Edge button5
95: 0 481ac000.gpio 5 Edge button3
126: 0 481ae000.gpio 3 Level wl18xx
141: 491 481ae000.gpio 18 Edge rf_irq_2
142: 1050 481ae000.gpio 19 Edge rf_irq_1
155: 30 INTC 72 Level 44e09000.serial
156: 3678 INTC 73 Level 48022000.serial
157: 2540 INTC 70 Level 44e0b000.i2c
158: 10134 INTC 64 Level mmc0
159: 274 INTC 28 Level mmc1
161: 0 INTC 77 Level wkup_m3
167: 0 INTC 75 Level rtc1
168: 0 INTC 76 Level rtc1
172: 434 INTC 41 Level 4a100000.ethernet
173: 29 INTC 42 Level 4a100000.ethernet
183: 1250 INTC 36 Level tilcdc
184: 64 INTC 16 Level TI-am335x-tsc, TI-am335x-adc
185: 0 INTC 109 Level 53100000.sham
187: 0 INTC 82 Level 4803c000.mcasp_tx
188: 0 INTC 83 Level 4803c000.mcasp_rx
189: 4 INTC 111 Level 48310000.rng
192: 1 INTC 18 Level musb-hdrc.1.auto
193: 95 INTC 19 Level musb-hdrc.2.auto
194: 149 INTC 17 Level 47400000.dma-controller
Err: 0
root@am335x-evm:~#
the result of "cat /sys/kernel/debug/gpio" is:
root@am335x-evm:~# cat /sys/kernel/debug/gpio
GPIOs 0-31, platform/44e07000.gpio, gpio:
gpio-5 (? ) out hi
gpio-7 (vtt ) out hi
gpio-16 (? ) out hi
gpio-19 (? ) out hi
gpio-20 (? ) out hi
gpio-21 (? ) out lo
gpio-28 (? ) out hi
GPIOs 32-63, platform/4804c000.gpio, gpio:
gpio-36 (button4 ) in hi IRQ
gpio-37 (? ) out lo
gpio-38 (? ) out lo
gpio-39 (? ) out lo
gpio-40 (sysfs ) in lo
gpio-41 (? ) out hi
gpio-44 (kim ) out hi
gpio-61 (wlan-en-regulator ) out lo
GPIOs 64-95, platform/481ac000.gpio, gpio:
gpio-64 (GPIO_LF_MOD ) out lo
gpio-65 (cd ) in lo IRQ
gpio-66 (button2 ) in lo IRQ
gpio-67 (button1 ) in lo IRQ
gpio-68 (button5 ) in hi IRQ
gpio-69 (button3 ) in lo IRQ
gpio-84 (? ) out lo
gpio-85 (? ) out lo
GPIOs 96-127, platform/481ae000.gpio, gpio:
gpio-100 (? ) out hi
gpio-114 (rf_irq_2 ) in lo IRQ
gpio-115 (rf_irq_1 ) in hi IRQ
gpio-116 (phy_reset ) out hi
gpio-117 (? ) out lo
GPIOs 480-487, i2c/0-0070, tca9554, can sleep:
GPIOs 488-495, i2c/0-0022, pcf8574, can sleep:
gpio-490 (sysfs ) out lo
gpio-491 (sysfs ) in hi
gpio-492 (sysfs ) in hi
gpio-493 (sysfs ) in hi
gpio-494 (sysfs ) in lo
gpio-495 (sysfs ) in hi
GPIOs 496-503, i2c/0-0021, pcf8574, can sleep:
gpio-496 (sysfs ) in lo
gpio-497 (sysfs ) in hi
gpio-498 (sysfs ) in lo
gpio-499 (sysfs ) in lo
gpio-500 (sysfs ) in lo
gpio-501 (sysfs ) in hi
gpio-502 (sysfs ) in hi
gpio-503 (sysfs ) in hi
GPIOs 504-511, i2c/0-0020, pcf8574, can sleep:
gpio-504 (reset_fg_i2c_mux ) out hi
gpio-505 (sysfs ) out lo
gpio-506 (sysfs ) out lo
gpio-507 (sysfs ) out lo
gpio-508 (sysfs ) out lo
gpio-509 (sysfs ) out lo
gpio-510 (sysfs ) out hi
gpio-511 (sysfs ) out lo
root@am335x-evm:~#
What can be the problem that mmc cd not send interrupt?
Thanks Oded