I am working on TMS320C6678 DDR3 layout SI simulation. I am using HyperLynx 9.1 as simulation tool and IBIS model, tms320C6678_4_2_1_r1p5b.ibs, download from ti website. When I try to run DDRx Batch simulation, I got following error,
Audit for the net: DSP_DDR3_CKP_0 with type: W1_Fast
** Error **: Too many drivers, not allowed in the DDR interface! Driving pins: U2500.A12, U2500.B12
** Info **: Initialization of drivers failed!
I checked the IBIS model file, it seems DDRCLKOUTP0/DDRCLKOUTN0 is not defined as differential pair which caused the problem.
Is the IBIS model from current product website correct?
Thanks,
-Yuan
PS: I found this post which has an IBIS model file tms320c6678_r1p6.ibs, which looks like be a newer version of IBIS model, anyone can confirm this file is legit to use? Thanks
https://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/188854