Other Parts Discussed in Thread: UNIFLASH
Hi All,
I am trying to flash SPL and u-boot flasher images onto the target by using the Ethernet interface and AM437x boot ROM code by changing the sysboot mode settings on both AM437x GP-EVM target and AM437x EVK platforms.
Here I am using the Uniflash tool for download the SPL and u-boot flasher images using the Ethernet interface. But it was failing to load this images. I have followed the below link to use and flash images using the Uniflash tool.
processors.wiki.ti.com/.../Sitara_Uniflash_Quick_Start_Guide
I have followed the below link to generate SPL and u-boot flasher images. In this link mentioned that patch (AM437x - [U-Boot Patch to Add TFTP Boot Configurations]) need to be apply to support flasher images (SPL, u-boot) for Ethernet/USB boot-mode, but this patch was not matching with the u-boot source which referred in the same link.
Example: From the patch one file is does not exit in the u-boot source, i.e "boards.cfg".
processors.wiki.ti.com/.../Sitara_Uniflash_Flash_Programming_with_Linux
I want to understand is there any u-boot source that can be download and use for flasher images instead of regular git u-boot source as mentioned in below link.
processors.wiki.ti.com/.../Linux_Core_U-Boot_User's_Guide
Could you please any one suggest me,
1. From where do I get the compatible working u-boot source for AM437x to generate SPL and u-boot flasher images.
2. Reference links which guide me the proper way to generate SPL flasher images for AM437x target platform and flash onto the target using the Uniflash tool(using interface Ethernet).
I appreciate your support on this.
Thanks for support in advance.
Thanks & Regards
Ch. Siva