Other Parts Discussed in Thread: AM3358
Dear All,
I am trying to boot my AM3358 Starter kit using SPI (winbond W25Q64FV) Flash. Till now I have successfully configured SPI with the kit and could easily write in SPI flash using Flash writing code provided with starterware. The problem is I am unable to boot it using SPI as the code for generating "boot_ti.bin" for AM335x starterkit is not available in starterware. Yes I do find a code for booting using SPI in am335x folder but it is very much specific for AM335x GP EVM module and is not working on SK(Starter kit) so I just stuck in the middle. Is it possible to boot directly from SPI without using Altera CPLD(installed on EVM module). If yes can anyone please guide me how to make correct "boot_ti.bin" file.
Note: My boot sequence is MMC0,SPI0,UART0,USB0
Best Regards
Ahmed