I will be using the MT29F2G08ABAGAH4-IT:G which is 256MB NAND flash with 8-bit address bus. I will also be booting from NAND flash. The DM385 has an 8-bit (GPMC_A[16 – 23]) and a 16-bit (GPMC_D[0 – 15]) address bus and the 16-bit bus has the boot mode pins on it. Here are my questions:
1.) Since I have an 8-bit address part do I need to use the 8-bit address on the DM385?
2.) Since I will be booting from NAND do I have to have my NAND flash connected to the BTMODE pins?
3.) If I have to use the BTMODE pins can I just use half of the bus for my part?