Hi TI Experts,
I am working on a SYS/BIOS project which needs to print float values to the console.
I figured out that the following statement has to be a part of the application .cfg file to enable the System_printf() to support printing of float values.
System.extendedFormats = '%$L%$S%$F%f';
But the System_printf() only prints 4 digits after the decimal point for the float values. I also used a precision specifier like "%.1f" or ""%0.2f"" in the format string of the System_printf(). That doesn't seem to work either.
Please let me know what more to be done to make the function print less than 4 digits after the decimal point.
Best regards.
Kaka