This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM572x USB1 is not working in U-boot and Linux

   Hi ,

         We Developed one custom board based on the TMDSEVM572X evm board. On EVM usb-0 is connected to USB hub chip and hub providing the three output ports. These three are working fine  on EVM. But in our design we are not using the USB hub, instead we directly connected to usb3.0 port.

We are using ti-processor-sdk-linux-am57xx-evm-02.00.01.07 which came along with TMDSEVM572X evm. with this SDK USB is not working in u-boot and Linux also. please suggest what all changes are required for our design.

while executing  "usb start" command  in u-boot , we are getting following log

U-Boot# usb start
starting USB...
scanning bus 0 for devices...   Couldn't reset port 1
1 USB Device(s) found
       scanning usb for storage devices...
 0 Storage Device(s) found

Regards

Kishor A