This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timing requirements for DM648 VLYNQ VCLK

Hi

Are the timing requirements for the VLYNQ VCLK the same as VPxCLKINx (Table 6-50 of SPRS372D.pdf)? 

Max speed is then ~100 MHz?

I'm scoping out the use of this port for transferring data to an FPGA for processing and need to know roughly what the max rate is. Xilinx states that their FPGAs are capable of 285 Mbps with bits on the VLYNQ interface (http://www.xilinx.com/support/documentation/ipbusinterfacei-o_processorbus_do-di-vlynq.htm)

Cheers

 

  • Eddie said:

    Are the timing requirements for the VLYNQ VCLK the same as VPxCLKINx (Table 6-50 of SPRS372D.pdf)? 

    Max speed is then ~100 MHz?

    The VLYNQ clock is actually seperate, the timing requirements for the VLYNQ are actually given in table 6-91 on page 166 of SPRS372E (DM648 Datasheet). Based on the spec, the VLYNQ must run at at least 125MHz (8nS max VCLK cycle time) but no more than 250MHz with the VCLK as input (pulse durations of 2nS minimum high/low) or nor more than 166MHz with the VCLK as output (pulse durations of 3nS minimum high/low).

    Eddie said:
    Xilinx states that their FPGAs are capable of 285 Mbps with bits on the VLYNQ interface

    This is probably with another device, different devices have different VLYNQ capabilities, keep in mind that the clocks mentioned above do not take into account any coding or protocol overhead so the actual bandwith is a bit less.

  • Dang, how did I miss that table! Sorry to bug you about it.

    So the max one directional rate is (4 bits * clk) - coding and protocol overhead. Any guestimates what the bps is?

    Thanks Bernie