Hi,
C5515 EVM Real Time Power Monitoring demo code is available. It can be downloaded from open source web site: http://code.google.com/p/c5505-ezdsp/
1. In the beginning it displays C5515 256 ROM characters in a few seconds.
2. Afterwards, power monitoring starts.It displays TI log in the LCD as well.
3. CPU running frequencies are changing from 12MHz to 120 MHz. It's showing the CPU running frequency, core current and core power consumption numbers.
4. At lower CPU speed, the LCD refresh time is slow. At higher CPU speed, the LCD refresh time is faster.
5. At lower CPU speed, the core current is low. At higher CPU speed, the core current is higher.

Regards,
Hyun