How to connect c6674(1.8V) with FPGA(3.3V) through EMIF? Which voltage-level shifter should I choose?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to connect c6674(1.8V) with FPGA(3.3V) through EMIF? Which voltage-level shifter should I choose?
Similarly, most FPGAs support I/O banks that can be powered either at 3.3V or 1.8V. Therefore, the simplest solution is connecting pins from the C6674 to an I/O bank configured for 1.8V operation. If you still need conversion, TI has many different kinds of level shifting devices. You would need to be more specific for us to pin-point a specific device. For example, TXS or TXB devices are useful for bidirectional level shifting. Little-logic devices like SN74LVC1T45 or the SN74AVC4T245 are useful either uni-directionally or for bi-directional operation when a direction control signal (i.e. R/W#) is available. Floating gate devices such as the PCA9306 are useful for bi-directional signals such as I2C. The C6678 EVM schematic contains examples of all of these. Please see the following link for detailed device selection support: .
Tom