Part Number: AM5728
Other Parts Discussed in Thread: TPD12S015, , DRA742
Tool/software: Linux
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5728
Other Parts Discussed in Thread: TPD12S015, , DRA742
Tool/software: Linux
Hi,
We tried quick hack patch removing the tpd12s015 driver from the chain of AM5 EVM and it worked fine. The patch just drops tpd12s015 from the dts, and the few GPIOs that were handled by tpd12s015, were changed to be handled by gpio-hog so that they are always enabled. So the SW thinks the SoC is directly connected to the HDMI connector now.
Attached tried patch on X15 and AM5 EVM. The patch isn't on top of 4.1 Processor SDK but on ti-linux-4.9.y branch of
git repo.
Below is the changes that were done -
REMOVED
----------------
&tpd12s015 {
gpios = <&gpio7 10 GPIO_ACTIVE_HIGH>, /* gpio7_10, CT CP HPD */
<&gpio2 30 GPIO_ACTIVE_HIGH>, /* gpio2_30, LS OE */
<&gpio7 12 GPIO_ACTIVE_HIGH>; /* gpio7_12/sp1_cs2, HPD */
};
ADDED
-------------
&gpio7 {
p10 {
/* gpio7_10, CT CP HPD */
gpio-hog;
gpios = <10 GPIO_ACTIVE_HIGH>;
output-high;
line-name = "CT CP HPD";
};
};
&gpio2 {
p30 {
/* gpio2_30, LS OE */
gpio-hog;
gpios = <30 GPIO_ACTIVE_HIGH>;
output-high;
line-name = "LS OE";
};
}
hdmi0: connector {
compatible = "hdmi-connector";
label = "hdmi";
type = "a";
hpd-gpios = <&gpio7 12 GPIO_ACTIVE_HIGH>;
port {
hdmi_connector_in: endpoint {
remote-endpoint = <&hdmi_out>;
};
};
If your are seeing "could not find video source" errors, it means that the previous component in the chain has not been registered. I.e. in TI GP EVM board, if hdmi connector gives that error, it means that tpd12s015 has not been probed successfully.
But this error may also be seen due to deferred probing even in a normal boot. I.e. if hdmi connector driver happens to be probed first, it can't find tpd12s015 because it's not loaded yet. After some time, tpd12s015 is probed, and then hdmi connector will be retried, successfully.
manisha,
Thank you for confirming the system/device tree would work without the TPD12S015 encoder defined -- A sanity check is always most useful! I ended up putting in a few more debugging statements in the various kernel drivers to see where things were failing and I now have the 4.9.41 kernel running on my board. In case others are using the Compulab AM572x boards the following is the configuration that worked for me - I have stripped out non-relevant bits so the config is easier to see - note in my case I'm just using HDMI.
Final configuration (kernel config) CONFIG_DRM_OMAP=y CONFIG_DRM_OMAP_WB=y CONFIG_OMAP2_DSS_INIT=y CONFIG_OMAP_DSS_BASE=y CONFIG_OMAP2_DSS=y CONFIG_OMAP2_DSS_DEBUG=y CONFIG_OMAP2_DSS_DEBUGFS=y # CONFIG_OMAP2_DSS_COLLECT_IRQ_STATS is not set CONFIG_OMAP2_DSS_DPI=y # CONFIG_OMAP2_DSS_VENC is not set CONFIG_OMAP2_DSS_HDMI_COMMON=y CONFIG_OMAP4_DSS_HDMI=y CONFIG_OMAP5_DSS_HDMI=y # CONFIG_OMAP2_DSS_SDI is not set # CONFIG_OMAP2_DSS_DSI is not set CONFIG_OMAP2_DSS_MIN_FCK_PER_PCK=0 CONFIG_OMAP2_DSS_SLEEP_AFTER_VENC_RESET=y CONFIG_TI_DSS6=y # # OMAPDRM External Display Device Drivers # # CONFIG_DRM_OMAP_ENCODER_OPA362 is not set # CONFIG_DRM_OMAP_ENCODER_TFP410 is not set # CONFIG_DRM_OMAP_ENCODER_TPD12S015 is not set # CONFIG_DRM_OMAP_ENCODER_TC358768 is not set # CONFIG_DRM_OMAP_DRA7_DIRECT_ENCODER is not set # CONFIG_DRM_OMAP_DRA7EVM_ENCODER_TPD12S015 is not set # CONFIG_DRM_OMAP_ENCODER_SII9022 is not set # CONFIG_DRM_OMAP_CONNECTOR_DVI is not set CONFIG_DRM_OMAP_CONNECTOR_HDMI=y # CONFIG_DRM_OMAP_CONNECTOR_ANALOG_TV is not set # CONFIG_DRM_OMAP_PANEL_DPI is not set # CONFIG_DRM_OMAP_PANEL_DSI_CM is not set # CONFIG_DRM_OMAP_PANEL_SONY_ACX565AKM is not set # CONFIG_DRM_OMAP_PANEL_LGPHILIPS_LB035Q02 is not set # CONFIG_DRM_OMAP_PANEL_SHARP_LS037V7DW01 is not set # CONFIG_DRM_OMAP_PANEL_TPO_TD028TTEC1 is not set # CONFIG_DRM_OMAP_PANEL_TPO_TD043MTEA1 is not set # CONFIG_DRM_OMAP_PANEL_NEC_NL8048HL11 is not set CONFIG_DRM_TILCDC=y CONFIG_DRM_TILCDC_SLAVE_COMPAT=y # CONFIG_DRM_QXL is not set # CONFIG_DRM_BOCHS is not set # CONFIG_DRM_VIRTIO_GPU is not set # CONFIG_DRM_FSL_DCU is not set CONFIG_DRM_BRIDGE=y Relevant Device Tree bits:
* I opted to not include the regulator definitions (ldoln_reg, ldo4_reg) to keep this doc concise / { aliases { display0 = &hdmi; }; hdmi_conn: connector { compatible = "hdmi-connector"; label = "hdmi"; type = "a"; hpd-gpios = <&gpio7 12 GPIO_ACTIVE_HIGH>; port { hdmi_connector_in: endpoint { remote-endpoint = <&hdmi_out>; }; }; }; }; &dra7_pmx_core { /* HDMI related pin configuration */ hdmi_pins: pinmux_hdmi_pins { pinctrl-single,pins = < DRA7XX_CORE_IOPAD(0x3808, PIN_INPUT | MUX_MODE1) /* i2c2_sda.hdmi1_ddc_scl */ DRA7XX_CORE_IOPAD(0x380c, PIN_INPUT | MUX_MODE1) /* i2c2_scl.hdmi1_ddc_sda */ >; }; hdmi_conn_pins: pinmux_hdmi_conn_pins { pinctrl-single,pins = < DRA7XX_CORE_IOPAD(0x37b8, PIN_INPUT | MUX_MODE14) /* spi1_cs2.gpio7_12 */ >; }; dss_dpi_pins: dss_pins { pinctrl-single,pins = < >; }; }; &dss { status = "ok"; pinctrl-names = "default"; vdda_video-supply = <&ldoln_reg>; }; &hdmi { status = "ok"; vdda-supply = <&ldo4_reg>; pinctrl-names = "default"; pinctrl-0 = <&hdmi_pins>; port { hdmi_out: endpoint { remote-endpoint = <&hdmi_connector_in>; lanes = <1 0 3 2 5 4 7 6>; }; }; }; &hdmi_conn { pinctrl-names = "default"; pinctrl-0 = <&hdmi_conn_pins>; };