Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
When debugging I see that function "iStat = ti_sysbios_timers_dmtimer_Timer_Instance_init__E(__obj, id, tickFxn, &__prms, __eb);" in file "app_pa8fg.c crashes with exception "CortxA8: Unhandled ADP_Stopped exception 0x20023". Everything worked before I installed the Code Composer Studio from 7.x to 7.2. As far as I know I didn't change the sources. After adding the timer source directly to the project I could see that it crahes in timer function "Void Timer_checkFreq(Timer_Object *obj)". But it is not easy to debug that because pausing manipulates the timer tick caluclation. Any ideas?
Regards,
David