Hi Kumar,
I have 4 different models which needs to be run on TDA2X. And to get real time performance of 30fps, I have done few calculations based on what each EVE Core computation power can provide in terms of Number of MACs?
As per the datasheet, EVE core at frequency of 530 MHz can provide 8 GMACs.
8 Giga MACs @ 1 fps
Aprox 500 Million MACs @ 15 fps
Aprox 250 Million MACs @ 30 fps
From the above calculation, If i design each deep learning model with less than 250 million MACS, Will all the 4 models can run at 30 fps concurrently on 4 EVE cores ?
Regards,
Sagar Kale