This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H06: Connection of EVMK2H and TMDXEVMPCI

Guru 15510 points
Part Number: 66AK2H06
Other Parts Discussed in Thread: TMDXEVMPCI, TMS320C6678, 66AK2H12,

Hi,

I have a question about EVMK2H and AMC-to-PCIe edge connector adapter(TMDXEVMPCI).
I know TMDXEVMPCI is for Keystone1 EVM and can't directly connect to EVMK2H.

AMC edge connector pin assignment of EVMK2H and Keystone1 EVM are same.
And it seem that format of AMC edge connector are same.

So, if I take off the heatsink and fan from the EVMK2H,
I guess TMDXEVMPCI can be connected to EVMK2H AMC edge connector.
Is it possible?

In the following E2E post,
TI employee said that TMDXEVMPCI is not compatible to EVMK2H.
And it seems that he is trying to say that RTM connector which are mounted next to
AMC edge connector will interfere the TMDXEVMPCI connection.
e2e.ti.com/.../392288

I checked the dimension of TMDXEVMPCI which I got from eInfochip.
As I compared with EVMK2H, I guess I could connect with TMDXEVMPCI.

If it is possible to connect EVMK2H and TMDXEVMPCI physically,
are there any other problem?

best regards,
g.f.