This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Champs,
I failed to DDR memory test and failed to access DDR memory.
Could you please check below customer's schematic DDR part?
GEL file I used is almost same with EVM's.
the blow is the error msg when I tried DDR3 memory test.
~~~~~`
CortexA15: Trouble Reading Memory Block at 0x80000000 on Page 0 of Length 0x4: (Error -1205 @ 0x80000000) Device memory bus has an error and may be hung. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
ddr3_write_read_test() cannot be evaluated.
Target failed to read 0x80000000
at temp=(ptr)[i] [evmk2g_arm.gel:1973]
at ddr3_memory_test() [evmk2g_arm.gel:2611]
at ddr3_write_read_test()CortexA15: Trouble Reading Register REG_SYSTEM_TARGET_CONFIG: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register REG_SYSTEM_MMU_CONFIG: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register REG_SYSTEM_MMU_STATUS: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register REG_SYSTEM_MMU_STATUS: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register CP15_Registers.REG_CTXA15_CP15_C2_TTBCR: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register CP15_Registers.REG_CTXA15_CP15_C2_TTBR0_64B: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register CP15_Registers.REG_CTXA15_CP15_C2_TTBR1_64B: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register CP15_Registers.REG_CTXA15_CP15_C3_DACR: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register REG_SYSTEM_MMU_STATUS: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register REG_SYSTEM_MMU_STATUS: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register CP15_Registers.REG_CTXA15_CP15_C2_TTBCR: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register CP15_Registers.REG_CTXA15_CP15_C2_TTBR0_64B: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register CP15_Registers.REG_CTXA15_CP15_C2_TTBR1_64B: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
CortexA15: Trouble Reading Register CP15_Registers.REG_CTXA15_CP15_C3_DACR: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
~~~~~~~~
DDR_RESET should be directly connected between K2G and DDR3 with the addition of pulled-down resister, right?
I captured from K2G schematic guide.
But, when I checked GP EVM schematic, it seemed DDR_RESET was connected with pull-up resister as below and I'm confused. Could you please make clarify on this?
Thanks and Best Regards,
SI.
We resolved this issue. We can access DDR3 memory using ICE_EVM.gel file, and it seemed the issue was occurred as they tried to access MSB 16bits which is no DDR memory connected. There is only 1 x 16bits memory connected in my customer's board same as ICE EVM, but we used GPEVM GEL file which enabled 32bit DDR3 memory i/f.
Thanks for your response and providing comments.
Thanks and Best Regards,
SI.