Hello,
Could you tell me whether the following understandings are correct or not for the definition of transient overshoot and undershoot at I/O terminal on AM3357?
In the datasheet, "Transient overshoot and undershoot specification at I/O terminal" is "25% of corresponding I/O supply voltage for up to 30% of signal period".
1.For VDDSHV6 (MIN: 3.135, TYP: 3.3V, MAX: 3.465V), must I/O terminal not exceed 4.33V (3.465V + 3.465V * 25% = 4.33V)?
2.Must the exceeded voltage of 3.465V be in the duration of 30% for the clock signal?
Best Regards,
Nomo