This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3352: DDR3 error

Part Number: AM3352

Tool/software: Linux

linux  memtester 25M:   

 high temperature error   

The last two bits of data bits are abnormal.

DDR3 LCDLR2 Need to be modified ?

  Checkerboard        : testing  25FAILURE: 0x55555555 != 0x555555aa at offset 0x000107df.

FAILURE: 0xaaaaaaaa != 0xaaaaaa55 at offset 0x000107e2.
FAILURE: 0x55555555 != 0x555555aa at offset 0x000107e3.
FAILURE: 0xaaaaaaaa != 0xaaaaaa55 at offset 0x000107e4.
FAILURE: 0x55555555 != 0x555555aa at offset 0x000107e5.
FAILURE: 0xaaaaaaaa != 0xaaaaaa55 at offset 0x000107e6.