Hi guys,
We need to execute a single kernel on different EVE cores with the following scenario.
1. The input image will be in x*y dimension.
2. It has to be broken into x1*y1, x2*y2, x3*y3 dimensions.
3. The kernel should be executed in all the EVE cores for these different image sections.
4. After the executions in all the cores completed, the individual outputs should be merged into x*y dimension single image.
And, the execution can be done with or without the support of VisionSDK.
Can you please suggest the steps or methodologies to do so.
Regards
Surbhi