Part Number: DP83822I
Other Parts Discussed in Thread: AMIC110
Tool/software: Linux
Hi, my company is evaluating the DP83822I as an ethernet PHY solution for an upcoming product, however we are having issues getting the PHY to function with the TI Linux drivers. I suspect we have an issue with our device tree configuration, and was hoping to find a reference device tree config for the TI driver. Does anyone know where I can find such a reference? We are using a Samsung Artik530S for our Linux module, but any embedded Linux reference using the DP83822 PHY should be helpful for us to determine the correct device tree configuration.
Below is a snippet of the relevant portion of our device tree as it is currently:
gmac0:ethernet@c0060000 {
pinctrl-names = "default";
pinctrl-0 = <&gmac_pins>;
status = "okay";
#address-cells = <0x1>;
#size-cells = <0x0>;
snps,phy-addr = <1>;
snps,reset-gpio = <&gpio_a 4 0>;
snps,reset-active-low;
snps,reset-delays-us = <0 100000 300000>;
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethernet_phy: ethernet-phy@1 {
reg = <3>;
fixed-link {
speed = <100>;
half-duplex;
};
};
};
};