Part Number: AM3352
Hi TI support,
On boot up but prior to OS (QNX is this case) loading, I have a requirement to ensure DDR3 contents (memory locations) are returned to a "blank" state - random, zeroes, or ones. Is it possible to gain access to DDR3 reset line during bootloader phase?
The desire behavior is to hold DDR3 in reset and/or disable any refresh cycle from occurring for 100ms prior to normal kernel code load sequence. Please advise if code executing in on-chip SRAM can access Sitara's DDR3 controller register to toggle the DDR3 reset line.
Thanks,
John