This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-DRA7X: GC320 : Alpha blending with multi-source blitting

Part Number: PROCESSOR-SDK-DRA7X

Tool/software: Linux

Hi,

My application requires to support upto 4 overlays upon the base video. We are making use of GC320 module available on Jacinto6.
The input format is ARGB and output format is YUYV.
Is it possible to perform alpha blending of these overlays while using multi-source blitting?
Is there an existing sample application that we could refer for this use-case.